Other Parts Discussed in Thread: DRV8711
Hi,
Im using the drv8711 evm with the gui to take a closer look at some torque regulations.
ST8918 from nanotech and measured to about 5 Amps at 13Nm with the origin hardware.
The supply is ratet at 48v and 10 Amps and testet with origin hardware.
My addaptive settings in the board are:
- Mode 1/128 Step
- Gain: 10
- Tourque 128 => makes 3,78 Amps
- Decmode: Fast Decay
- Target Speed: 26880 pps => makes 63 rpm with 1,8° / step
- the rest of settings are default
The Operation:
- everything on startup is normal the motor reached the 63 rpm with about 2Nm
The Issue:
- Until about 3-1 min the motor stops suddenly with the bpdf fault.
- This issue is repeadable and clearable by clearing the bpdf bit in the statusregister (0x07)
Questions:
- does the evaluation module could give out 5 amps ? The datasheet doesnt say anything about that. (the mosfets coud give 5 Amps)
- What conditions relay to the predriver fault ? THe datasheet only tells something about exessive current is detected but not how much is it and what could i do to prevent this
- the issue feels like a heat problem, because the time of the fault is shoten by fast clearing the register and repead. Is there any connection?
- Could you give me some hints to optimise the motor to 10Nm 5Amps ?
Thanks, Johannes