Hi Champs
Could you please help clarify/confirm on max J6 capablites
- Max DDR3 size that can be connected to 2 EMIFs on J6 – Is it 2GB * 2 = 4GB?
- Can the MMC interface be used to connect 16GB memory? or 32GB SD Cards?
Best Regards
Feroz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Champs
Could you please help clarify/confirm on max J6 capablites
Best Regards
Feroz
Irfan, Dobrin,
SDSC and SDHC are both supported under the current SW. SDXC uses exFAT, which is a Windows proprietary filesystem. If customer/SW has the corresponding driver integrated they can interact with SDXC cards and develop MMC code on top of it.
J6 ROM does not handle exFAT format, hence SDXC is not supported in the ROM stage.
Thanks & Regards,
Shiou Mei
*Updated with clarification