This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA746: Wayland/Weston and Pipeline/Plane/Overlay usage

Part Number: DRA746

Tool/software: Linux

Dear Team,

We have below query regarding overlay/pipeline/plane (i.e. 1 GFX and 3 VID) of DRA746.  Our s/w is based on SDK 3.02.00.03

1. How can we select/use particular pipeline for specific application while we are using wayland-ivi-extesnion (with ivi-controller.so) and wayland/weston (with ivi-shell and drm backebd )? Is there anyway or configuration or code changes?

For example

HMI on GFX using A15 core

Navigation  on VID1 uisng A15 core

VideoPlayer on VID1 uisng A15 core

Browser on VID1 uisng A15 core

Camera1 app on VID2 using M4 core

Camera2 app on VID3 using M4 core

Thanks & Regards,

Vikash