Other Parts Discussed in Thread: DRA742
Our custom board using DRA742 and connect to QSPI flash(STMicro N25Q128) with QSPI_1. At older BSP version(7.04.00.03), after i modify dts file and ti-qspi.c(change quad_read setting for STMicro), i can normally access flash and using QSPI boot. But after i use new BSP version(3.02.00.03), i can't access flash normally even i modify dts file and ti-qspi.c.
Finally, i can access flash normally after i disable "set_quad_mode()" at spi_flash_scan() in spi_flash.c. After i write MLO & u-boot.img to flash through "sf" command, i switch boot mode to QSPI boot, but boot fail.
The log show =>
U-Boot SPL 2016.05 (Aug 23 2017 - 18:11:04) DRA752-GP ES2.0 ** First descriptor is NOT a primary desc on 1:1 ** *** Warning - bad CRC, using default environment Trying to boot from SPI (1)quad support!!! GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645 part_get_info_efi: *** ERROR: Invalid GPT *** GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645 part_get_info_efi: *** ERROR: Invalid Backup GPT *** cannot find partition: 'environment' SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ###
Is ther exist new QSPI boot method for new BSP version(3.02.00.03)? What's the error message mean?
Regards,
Shawn