This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA72XEVM: failed to compile /ti-processor-sdk-linux-automotive-dra7xx-evm-03_04_00_03

Part Number: DRA72XEVM

Tool/software: Linux

Dear,

I got following errors during executing build-core-sdk.sh. how to fix this problem?

logan@logan-HP-Notebook:~/sda3/ti/ti-processor-sdk-linux-automotive-dra7xx-evm-03_04_00_03/yocto-layers$ ./build-core-sdk.sh dra7xx-evm
[PSDKLA]>
[PSDKLA]> Current Directory is /home/logan/sda3/ti/ti-processor-sdk-linux-automotive-dra7xx-evm-03_04_00_03/yocto-layers
[PSDKLA]> PATH is /home/logan/sda3/programs/jdk1.8.0_151/bin:/home/logan/sda3/programs/jdk1.8.0_151/jre/bin:/usr/local/cuda-9.0/bin:/home/logan/sda3/ti/PROCESSOR_SDK_VISION_03_02_00_00/ti_components/cg_tools/linux/ti-cgt-c6000_8.2.2/bin:/home/logan/bin:/home/logan/.local/bin:/home/logan/sda3/ti/PROCESSOR_SDK_VISION_03_02_00_00/ti_components/os_tools/linux/linaro/gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf/bin/:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin
[PSDKLA]> Building on logan-HP-Notebook running Linux logan-HP-Notebook 4.13.0-26-generic #29~16.04.2-Ubuntu SMP Tue Jan 9 22:00:44 UTC 2018 x86_64 x86_64 x86_64 GNU/Linux
[PSDKLA]> Starting Yocto build at 2018年 02月 26日 星期一 14:25:14 CST
[PSDKLA]>
[PSDKLA]> cd build
[PSDKLA]> . conf/setenv
[PSDKLA]> cp conf/local.conf conf/local.conf.pristine
[PSDKLA]> MACHINE=dra7xx-evm bitbake tisdk-rootfs-image
NOTE: Started PRServer with DBfile: /home/logan/sda3/ti/ti-processor-sdk-linux-automotive-dra7xx-evm-03_04_00_03/yocto-layers/build/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 45445, PID: 3336
Loading cache: 100% |##############################################################################################| ETA:  00:00:00
Loaded 2849 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION        = "1.30.0"
BUILD_SYS         = "x86_64-linux"
NATIVELSBSTRING   = "Ubuntu-16.04"
TARGET_SYS        = "arm-linux-gnueabi"
MACHINE           = "dra7xx-evm"
DISTRO            = "arago"
DISTRO_VERSION    = "2016.12"
TUNE_FEATURES     = "arm armv7a vfp thumb neon       callconvention-hard"
TARGET_FPU        = "hard"
meta-glsdk        = "HEAD:66cfd8ef55344508d6e7b306259f34c05b828194"
meta-arago-distro
meta-arago-extras = "HEAD:4c01410ffde8853224567fb6078d7d9f190b942f"
meta-qt5          = "HEAD:f8584d7a7c90afc71484a40279aa3df651d0e04f"
meta-networking   
meta-ruby         
meta-python       
meta-oe           = "HEAD:55c8a76da5dc099a7bc3838495c672140cedb78e"
meta-ti           = "HEAD:5f3a1169d307fec41626f850f5c700437dedbe93"
meta-linaro-toolchain
meta-optee        = "HEAD:2f51d38048599d9878f149d6d15539fb97603f8f"
meta              = "HEAD:bfa04fa71c47e8fe9528208848cfcec2e232777d"

NOTE: Preparing RunQueue
WARNING: /home/logan/sda3/ti/ti-processor-sdk-linux-automotive-dra7xx-evm-03_04_00_03/yocto-layers/sources/meta-arago/meta-arago-distro/recipes-core/images/tisdk-rootfs-image.bb.do_compile is tainted from a forced run
WARNING: /home/logan/sda3/ti/ti-processor-sdk-linux-automotive-dra7xx-evm-03_04_00_03/yocto-layers/sources/meta-arago/meta-arago-extras/recipes-graphics/omapdrmtest/omapdrmtest_1.0.0.bb.do_compile is tainted from a forced run
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: hevc-arm-decoder-01.00.00.01-r3 do_fetch: Failed to fetch URL gforge.ti.com/.../REL.HEVC.D.ARM.OBJ.01.00.00.01.tar.gz, attempting MIRRORS if available
ERROR: hevc-arm-decoder-01.00.00.01-r3 do_fetch: Fetcher failure: Fetch command failed with exit code 4, output:
failed: Connection timed out.
failed: Connection timed out.

ERROR: hevc-arm-decoder-01.00.00.01-r3 do_fetch: Function failed: Fetcher failure for URL: 'gforge.ti.com/.../REL.HEVC.D.ARM.OBJ.01.00.00.01.tar.gz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/logan/sda3/ti/ti-processor-sdk-linux-automotive-dra7xx-evm-03_04_00_03/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/hevc-arm-decoder/01.00.00.01-r3/temp/log.do_fetch.3383
ERROR: Task 3008 (/home/logan/sda3/ti/ti-processor-sdk-linux-automotive-dra7xx-evm-03_04_00_03/yocto-layers/sources/meta-arago/meta-arago-extras/recipes-multimedia/hevc-arm-decoder/hevc-arm-decoder_01.00.00.01.bb, do_fetch) failed with exit code '1'