Part Number: DRA74
Hi
There are some video input port questions,
1.We use vin3a & vin4b to receive BT656 format signals( clk, D[0:7], but we could only recognize H/L by GPIO,
not in video format. Is there any setting besides these pinmux of their 9 pins needed
Pins of vin3a:B11,B7,B8,A7,A8,C9,A9,B9,A10
Pins of vin4b: N9,P5,R5,R9,P6,T7,T6,T9,R6
2.We use vin2a to receive 480p 24 bits DRGB signals( DE, H/V, clock, D[0:23])
How to set it reading in DE-mode(DE,clk,data) or HV-mode(H/V,clk,data)?
Is the resolution should be set before?