This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2E: A15 core is dead when running 4 camera streaming on tda2x after 3-4 minutes

Part Number: TDA2E

Hi,

I am running 4 camera streaming on tda2x but after running fine for 3-4 minutes a15 core is dead

and camera streaming stopped.Following are the ndk/nsp package versions that i am using

nsp_gmacsw_4_12_00_00

ndk_2_24_00_11.

Configuring ndk for 1 gbps.

I have also doubt reagrding below parameters.

#define NDK_TX_PACKET_TASK_PRI (14)//OS_TASKPRIHIGH

#define NDK_TX_PACKET_TASK_STACK (2048)

#define NDK2NSP_TX_PACKETS (128U)
#define NDK2NSP_RX_PACKETS (64U)

Will there be change in default values if we are streaming 4 cameras 1280x800 resolution.

How can i determine the values based on my rquirement.

Will the modification of above parameter values make the system more stable.

Regards

Mayank