Part Number: TDA2E
Hi all,
I am trying to run the lane detection sample programs in Vision_sdk in TDA2x board.
We found two samples available inside vision_sdk toolkit.
1. One is under use case directory
"VISION_SDK_02_12_00_00\vision_sdk\examples\tda2xx\src\usecases\vip_single_cam_lane_detection"
2. Another under the following directory.
"C:\VISION_SDK_02_12_00_00\ti_components\algorithms_codecs\REL.200.V.LD.C66X.00.02.03.00\200.V.LD.C66X.00.02\modules\ti_lane_detection\test"
Can anyone please explain us the difference between the two sample application. How can we use those for further development.
I tried running both the samples.
I am not clear on the output of the sample applications.
The Lane Detection example under use-case is showing the video with some zebra lines marking on the Lane, only on the single side.
Can anyone explain the actual output showing?
Another example is getting the individual monochrome frames as input and giving (x,y) co-ordinates as output.
How can send video input for this use-case and how can we see the output of these frames and process further.
How can I modify the algorithm to tune the lane detection as per my requirement.
Can somebody please help me on this, as I am new to this.
Thanks.
Suganthi