Dear Experts,
could You please confirm which guaranteed temperature accuracy the internal temperature sensors on TDA3x device have over lifetime?
I could not find any reference in DM/TRM.
In TDA2x TRM +/- 2 degC are mentioned as a side note for TSHUT:
"The value for the high TSHUT threshold is 123°C (assuming ±2°C temperature sensor accuracy), and the low TSHUT threshold is 105°C."
Best Regards,
Gregor