Tool/software: Linux
Hi There,
I am using VSDK_03_01_00_00 with TDA2XX SOC and want to execute some networking related use cases . So I have referred "VisionSDK_UserGuide_NetworkTools.pdf" PDF for primary setup such as setting the static IP but in this document they have mentioned a "Note" under the Introduction section as "these tools can be used only when BIOS based NDK/NSP runs on target".
So please confirm do we have support of these tools with "Linux+ Bios" too or it is only for "BIOS".
@NOTE:- If these tools are only for "BIOS" then how the "HOST" and "EVM" board will establish the communication, if the build is "Linux+Bios"?.
Regards,
Anshul Jain.