Part Number: TDA2EVM5777
Tool/software: TI-RTOS
We are trying to use the sample use case (null_src_dec_display) with our generated data.
The data file is created from the following MKV file: http://jell.yfish.us/media/jellyfish-20-mbps-hd-h264.mkv
To remove the MKV container and output .h264 bitstream, we used the following command:
ffmpeg -i jellyfish-20-mbps-hd-h264.mkv -an -vcodec libx264 -bf 0 -vstats_file h264.stat 1920x1080_00.h264
We then created the binary index of frame sizes using h264.stat to create 1920x1080_00.hdr.
From here we perform minor modifications in the source code to match the input as follows:
#define ENCDEC_MAX_FRAME_WIDTH (1920)
#define ENCDEC_MAX_FRAME_HEIGHT (1080)
...
strncpy(pPrm->channelParams[chId].nameDataFile, "1920x1080_00.h264", 260);
strncpy(pPrm->channelParams[chId].nameIndexFile, "1920x1080_00.hdr", 260);
We are able to play the video correctly, but there are green artifacts in the images as shown in the attached image below:
Is there other configurations in use case that we missed and we need to change in order to display the video correctly?