This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TDA2P-ACD: CSI2 PHY RESET_DONE is not coming

Part Number: TDA2P-ACD


Tool/software: TI-RTOS

Hi,

We are using CSI2 for camera sensor interface but after issuing Reset of the complex IO (CAL_CSI2_COMPLEXIO_CFG[30].RESET_CTRL) we are not getting RESET_DONE (CAL_CSI2_COMPLEXIO_CFG[29].RESET_DONE remains 0) even though the external camera sensor is giving MIPI HS clock properly.

We are using 4-lane configuration (lane 4: clock, lane 1/2/3/5: data) and below is the register dump after reset:

CAL_CSI2_COMPLEXIO_CFG_0 (0x489b 0304) = 0x4A053214

CAL_CSI2_PPI_CTRL_0 (0x489B 0300) = 0x00000009

CTRL_CORE_CONTROL_CSI (0x4A00 26DC) = 0xF8000900

REG0 (0x489B 0800) = 0x0000082E

REG1 (0x489B 0804) = 0xC002E116

Clock/Power domain registers:

Any points to check?

Regards,

James

  • Adding Clock/Power domain registers:
    CM_CAM_CLKSTCTRL = 0x00001702
    CM_CAM_STTICDEP = 0x00000030
    CM_CAM_VIP1_CLKCTRL = 0x00000001
    CM_CAM_VIP2_CLKCTRL = 0x0x00000001
    CM_CAM_VIP3_CLKCTRL = 0x00040001
    CM_CAM_CSI1_CLKCTRL = 0x00040001
    CM_CAM_CSI2_CLKCTRL = 0x00040001
    PM_CAM_PWRSTCTRL = 0x00030000
    PM_CAM_PWRSTST = 0x00000037

    Regards,
    James
  • Hi James,

    Can i know the software that you are using?

    Also, can you please check on the following
    1. CSI2 Clock configuration, the CSI2 clock from the sensor has to match the CSI2/DDR clock configured in CAL.
    2. Can you ensure the lane ordering is correct, i.e. clock lane and data lanes are correctly mapped. Also check on the polarity mapping
    3. Can you read some register in the sensor to check if frames are indeed being sent

    Regards,
    Sujith
  • Hi Sujith,

    We are using VSDK 3.02.
    1. For CSI2 Clock configuration, camera sensor is outputting 400 MHz which is our default configuration - so, I think there will be no issues in CSI2/DDR clock configuration in CAL but will double check and let you know.
    2. Lane ordering and polarity mapping: lane4 - clock, lane1/2/3/5 - data
    Confirmed the clock is connected to lane 4
    3. Will check sensor registers to confirm if frames are being sent and let you know - we could see the frames are coming from sensor through oscilloscope probing.

    In TDA2Px TRM, I could see the comments:
    For the CAL_CSI2_COMPLEXIO_CFG_l[29] RESET_DONE bit to be set to
    0x1 (reset completed), the external sensor must to be active and sending
    the MIPI HS BYTECLK.

    Please let me know if you have any other points to check since I could see the clock is coming from sensor - by probing clock lane with the scope.

    Regards,
    James
  • Hi James,

    The issue seems to be position of the clock lane, below is extract from TDA2Px TRM.

    Regards, Sujith

  • Hi Sujith,

    Sorry for the confusion.
    In my description, I'm following the index from the VSDK 3.02 source code which starts from 1 (not 0).
    So, if I follow the indexing in TDA2Px TRM: clock- lane3, data- lane0/1/2/4.

    Regards,
    James
  • Hi James,

    OK, i understand. Which sensor / camera module are you using?
    Also, please ensure to start video streaming on the camera module just before you start CAL/Reception on TDA2Px.

    Please cross check the CSI2 Clock from the sensor.

    Regards,
    Sujith
  • Hi Sujith,

    It's AR0231 2M sensor.
    Will check the timing and let you know but what could be a best timing to start video streaming when you say just before CAL?
    Do you expect any problems if we start streaming much earlier than expected?

    Regards,
    James
  • Hi James,

    MIPI performs a initial handshake before switching to high speed transmission mode. Once the termination is enabled on the lanes, there is definite timeout before switching to high-speed transmission mode. (Standard DPHY / MIPI sequence)

    Please refer single channel CAL/CSI2 based usecases. The CAL is configured and before the function call to start reception, the sensor would be programmed and transmission enabled and CAL / CSI2 receiver is started.

    Please refer file \apps\src\rtos\usecases\iss_capture_isp_simcop_display\chains_issIspSimcop_Display.c function chains_issIspSimcop_Display_StartApp ().

    Function appStartIssSensorSerDes () Starts the sensor and function call chains_issIspSimcop_Display_Start () starts reception via CSI2 / Capture Link.

    Regards,
    Sujith
  • Hi Sujith,

    I'm running chains_csi2CalMultiCam_View usecase and in chains_csi2CalMultiCam_View_StartApp(), camera sensor starts video streaming before chains_csi2CalMultiCam_View_Start() gets called but RESET_DONE is not coming yet in CAL_CSI2_COMPLEXIO_CFG register.

    Regards,
    James
  • Hi James,

    If you have set the Capture Link parameters as per the lanes connected and CSI2 clock provided by the camera. It should have worked. Can you please check if the sensor configuration is working with any other board.

    Also, if you have camera module/EVM that is supported by VisionSDK, you could ensure EVM is fine.

    Regards,
    Sujith
  • Hi Sujith,

    I tested the use case on TDA2Px EVM with Fusion Kit (OV2775 sensor) and could see the RESETDONECTRLCLK (bit 29) was set first in REG1 register and after that, as soon as BYTECLK was received from sensor (through deserializer) RESETDONERXBYTECLK (bit 28) was set (REG1: 0xE002E116 --> 0xF002E116).

    But on the customer board, REG1 register value is 0xC002E116 which means CTRLCLK is not provided to CSI2 PHY from PRCM.

    The clock tree is: CTRLCLK <-- LVDSRX_96M_GFCLK <-- FUNC_96M_FCLK <-- FUNC_192M_CLK <-- DPLL_PER [CLKOUTX2_M2].

    So I checked below registers on the customer board but could not see any suspicious points:

    1. CM_CLKMODE_DPLL_PER(0x4A00 8140) = 0x07
         DPLL_EN = 7 (Enables the DPLL in Lock mode)
    2. CM_DIV_M2_DPLL_PER(0x4A00 8150) = 0x0804
        CLKX2ST = 1 (The clock output is enabled)
        DIVHS = 4 (M2)
    3. CM_CLKSEL_DPLL_PER(0x4A00 814C) = 0x6004
        DPLL_MULT = 96
        DPLL_DIV = 4

    Could you let me know from what points/registers should I check to confirm if CTRLCLK is provided properly from  PRCM?

    FYI, CTRLCLK is enabled in Control Module as you  can see in my first posting.

    CTRL_CORE_CONTROL_CSI (0x4A00 26DC) = 0xF8000900

    Regards,

    James

  • Hi James,

    Once the clock from the CSI2 source is detected and locked on, the byte clock is generated. In this case, i doubt the de-serailizer configuration.

    Can you please check if you could operate de-serilizer in "continuous clock mode"

    Regards, Sujith

  • Hi Sujith,

    Yes, that's for BYTECLK which is coming from camera sensor (externally) but I'm not sure why the CTRLCLK which is the control clock for CSI2 PHY module coming from PRCM is not set properly on customer board.

    Regards,
    James
  • Hi James,

    As we are discussing this issue offline, can we mark this thread as closed. Once resolved, we could post the solution into this thread?

    Regards,
    Sujith
  • Hi Sujith,

    The issue was resolved by enabling de-serializer after we completed CSI2 PHY initialization.
    Previously, de-serializer was enabled (and CSI2 clock and data was being provided) before CSI2 PHY initialization and it was preventing CSI2 PHY reset.
    Thanks for your support and please feel free to add comments if you have any.

    Regards,
    James