This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2: Running a model on multiple cores

Part Number: TDA2

Hi,

As per my understanding in the config file, we have option to select EVE or DSP core by selecting layersGroupId(1 for EVE and 2 for DSP). In case, if the model is to be run on multiple EVE cores, say EVE1 and EVE2(first few layers on EVE1 and next few layers on EVE2), is there any way to mention this from the config file?

Thanks in advance,

Navinprashath.R.R 

  • Yes, we can do that by assigning unique layersGroupId for each of the cores, let's say 1 for EVE1, 2 for EVE2, 3 for EVE3 and 4 for DSP.

    Note that this layersGroupIds 1 for EVE and 2 for DSP is just an example, you can assign any unique layersGroupId and same mapping should used in running inference.

    Thanks,
    Praveen