Part Number: TDA2PXEVM
Tool/software: Linux
Dear TI,
we have two Intel Optane 900P NVMe SSD's - one is 2.5" U.2 and the other is HHHL Form Factor.
We connected the SSD to TDA2P EVA board and we have issues regarding the write speed (this applies too both SSD's).
The SSD is connected over PCIe and the EVA board sees the SSD as GEN2 x2 PCIe device.
When we use dd command to write data to the SSD, we get on average 200MBps write speed.
The dd command is as follows:
dd if=/dev/zero of=/run/media/nvme0n1p1/test.raw bs=128k count=10k
We tested both SSD's on two different PC's (one PC has a GEN2 PCIe controller and the other one has a GEN3 PCIe controller).
In both cases the write speed was on average 1.4GBps. On PC the SSD is configured as GEN2 or GEN3 x4 PCIe device.
Based on the test results on PC, we where expecting to get 600MBps ~ 700MBps write speed when we use the EVA board.
Can you help us with this issue?
Regards,
Stefan