Other Parts Discussed in Thread: AM1808, OMAP-L138, AM1810
Hi There,
This is regarding - Compatibility between AM1808 and OMAP L138.
It is said that, AM1808 and OMAP L138 are Pin to Pin and Software compatible - Thus Can any body address following items :
1. "Having Software and Pin Compatible"Does it mean that any board designed around AM1808 will work as is [without any changes] with OMAP L138 by just replacing AM1808 by OMAP L138?
2. If answer for # 1 is YES - I don't have any query but if NO Then -
2.1 What are the things must be taken care or provision must be there on board to make a board compatible for both AM1808 and L138
2.2 Is there any document available from TI which shows the changes required for replacing from AM1808 with OMAP L138 and vice-a-versa ?
Thanks & Regards,
Rizwan Hirani