This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPMC interface to external memory device (FPGA)



We are interfacing an FPGA as a 16bit wide memory device ising the GPMC.

We have used the info as indicated below to have our system work, but we have some issues.

The configuration of the GPMC is rather involved, and we have tweaked it in order to satify our timen requirements.

 We have not optimized the timings yet.

Our test software produces two 16 bit wide writes, and we are OK with this.

In the case of read operations, a single 16 bit wide read transaction is produced,

and to actually receive the correct data, we need two reads.

Could any one please suggest what is happening here , and a way to resolve it ?

My impression is that we have a GPMC parameter wrong.

I'll post the configuration parameters in a follow up post.

 

Thanks, Jure Z.

 

=======================================================================================

We used the info in the thread:

http://e2e.ti.com/support/dsp/sitara_arm174_microprocessors/f/791/p/176492/643640.aspx#643640http://e2e.ti.com/support/dsp/sitara_arm174_microprocessors/f/791/t/190352.aspx

which points to the example file:

1641.GPMC_DRAM_example.zip

 

 

  • These are the parameters, sniping some of the code:

     

    //## GPMC_CONFIG1 // configure for NOR and granularity x2

    temp = 0x01200; // device type 16 bit wide

    HWREG(SOC_GPMC_0_REGS + GPMC_CONFIG1(csNum)) = temp;

     

    //## GPMC_CONFIG2

    temp = 0x070B00;

    HWREG(SOC_GPMC_0_REGS + GPMC_CONFIG2(csNum)) = temp;

     

    //## GPMC_CONFIG3

    temp = 0x020200;

    HWREG(SOC_GPMC_0_REGS + GPMC_CONFIG3(csNum)) = temp;

     

    //## GPMC_CONFIG4

    temp = 0x07050606;

    HWREG(SOC_GPMC_0_REGS + GPMC_CONFIG4(csNum)) = temp;

     

    //## GPMC_CONFIG5

    temp = 0x08070A;

    HWREG(SOC_GPMC_0_REGS + GPMC_CONFIG5(csNum)) = temp;

     

    //## GPMC_CONFIG6

    temp = 0x07040000;

    HWREG(SOC_GPMC_0_REGS + GPMC_CONFIG6(csNum)) = temp;

     

    //## GPMC_CONFIG7

    temp = 0x0F49;

    HWREG(SOC_GPMC_0_REGS + GPMC_CONFIG7(csNum)) = temp;

  • and here is a more detailed table using the TRM table format:

    7.1.5.11 GPMC_CONFIG1_i

    The configuration 1 register sets signal control parameters per chip select.

    Table 7-65. GPMC_CONFIG1_i Field Descriptions

    31 WRAPBURST: 0 Synchronous wrapping burst not supported

    30 READMULTIPLE: 0 single access

    29 READTYPE: 0 Read Asynchronous

    28 WRITEMULTIPLE: 0 Single access

    27 WRITETYPE: 0 Write Asynchronous

    26-25 CLKACTIVATIONTIME : 0 First rising edge of GPMC_CLK at start access time

    24-23 ATTACHEDDEVICEPAGELENGTH : 0 4 Words

    22 WAITREADMONITORING :0 WAIT pin is not monitored for read accesses

    21 WAITWRITEMONITORING : 0 WAIT pin is not monitored for write accesses

    20 Reserved 0 Reserved

    19-18 WAITMONITORINGTIME : 0 WAIT pin is monitored with valid data

    17-16 WAITPINSELECT :0 WAIT input pin is WAIT0

    15-14 Reserved 0 Reserved

    13-12 DEVICESIZE 1h 16 bit

    11-10 DEVICETYPE :0 NOR Flash like, asynchronous and synchronous devices

    9-8 MUXADDDATA : 2h Address and data multiplexed attached device

    7-5 Reserved 0 Reserved

    4 TIMEPARAGRANULARITY : 0 ×1 latencies

    3-2 Reserved : 0 Reserved

    1-0 GPMCFCLKDIVIDER : 0 GPMC_CLK frequency = GPMC_FCLK frequency

    ------------------------------------------------

    7.1.5.12 GPMC_CONFIG2_i

    Chip-select signal timing parameter configuration.

    Table 7-66. GPMC_CONFIG2_i Field Descriptions

     

    31-21 Reserved 0 Reserved

    20-16 CSWROFFTIME : 7 GPMC_FCLK cycles

    15-13 Reserved 0 Reserved

    12-8 CSRDOFFTIME :0xB GPMC_FCLK cycles

    7 CSEXTRADELAY : 0 CS i Timing control signal is not delayed

    6-4 Reserved 0 Reserved

    3-0 CSONTIME 0 0 GPMC_FCLK cycle

    -----------------------------------------------------

    7.1.5.13 GPMC_CONFIG3_i

    ADV# signal timing parameter configuration.

    Table 7-67. GPMC_CONFIG3_i Field Descriptions

     

    31 Reserved 0 Reserved

    30-28 ADVAADMUXWROFFTIME : 0 0 GPMC_FCLK cycle

    27 Reserved 0 Reserved

    26-24 ADVAADMUXRDOFFTIME : 0 0 GPMC_FCLK cycle

    23-21 Reserved 0 Reserved

    20-16 ADVWROFFTIME : 2 GPMC_FCLK cycles

    15-13 Reserved 0 Reserved

    12-8 ADVRDOFFTIME : 2 GPMC_FCLK cycles

    7 ADVEXTRADELAY : 0 ADV Timing control signal is not delayed

    6-4 ADVAADMUXONTIME : 0 0 GPMC_FCLK cycle

    3-0 ADVONTIME : 0 0 GPMC_FCLK cycle

    ---------------------------------------------------------

    7.1.5.14 GPMC_CONFIG4_i

    WE# and OE# signals timing parameter configuration.

    Table 7-68. GPMC_CONFIG4_i Field Descriptions

     31-29 Reserved 0 Reserved

    28-24 WEOFFTIME : 7 GPMC_FCLK cycles 

    23 WEEXTRADELAY : 0 WE Timing control signal is not delayed

    22-20 Reserved 0 Reserved 

    19-16 WEONTIME : 5 GPMC_FCLK cycles

    15-13 OEAADMUXOFFTIME : 0 0 GPMC_FCLK cycle 

    12-8 OEOFFTIME : 6 GPMC_FCLK cycles

    7 OEEXTRADELAY : 0 OE Timing control signal is not delayed 

    6-4 OEAADMUXONTIME : 0 0 GPMC_FCLK cycle

    3-0 OEONTIME : 6 GPMC_FCLK cycle

     ------------------------------------------------

    7.1.5.15 GPMC_CONFIG5_i

    RdAccessTime and CycleTime timing parameters configuration.

    Table 7-69. GPMC_CONFIG5_i Field Descriptions

     

    31-28 Reserved 0 Reserved

    27-24 PAGEBURSTACCESSTIME : 0 0 GPMC_FCLK cycle

    23-21 Reserved 0 Reserved

    20-16 RDACCESSTIME : 0xA GPMC_FCLK cycles

    15-13 Reserved 0 Reserved

    12-8 WRCYCLETIME : 7 GPMC_FCLK cycles

    7-5 Reserved 0 Reserved

    4-0 RDCYCLETIME : 0xA GPMC_FCLK cycles

    ---------------------------------------------------------

    7.1.5.16 GPMC_CONFIG6_i

    Table 7-70. GPMC_CONFIG6_i Field Descriptions

    31-29 Reserved 0 Reserved

    28-24 WRACCESSTIME : 7 GPMC_FCLK cycles

    23-20 Reserved 0 Reserved

    19-16 WRDATAONADMUXBUS : 4

    15-12 Reserved 0 Reserved

    11-8 CYCLE2CYCLEDELAY :0 0 GPMC_FCLK cycle

    7 CYCLE2CYCLESAMECSEN :0 No delay between the two accesses

    6 CYCLE2CYCLEDIFFCSEN :0 No delay between the two accesses

    5-4 Reserved 0 Reserved

    3-0 BUSTURNAROUND : 0 0 GPMC_FCLK cycle

     

    -----------------------------------------------------

    7.1.5.17 GPMC_CONFIG7_i

    Chip-select address mapping configuration.

    Table 7-71. GPMC_CONFIG7_i Field Descriptions

     

    31-12 Reserved 0 Reserved

    11-8 MASKADDRESS 0xF Chip-select size of 16 Mbytes

    7 Reserved 0 Reserved

    6 CSVALID : 1 CS enabled

    5-0 BASEADDRESS : 9 Chip-select base address.

    ========================================================= 

  • What happens on the bus?  You'll need to look at the resulting transfers/timing to understand the root of the issue.  For starters, are you seeing both accesses on the bus?  Is the FPGA returning invalid data for the first read, but valid data for the second read?

  • on the read cycles, the processor drives the bus with stale data, data being correct for the previous access.

    a workaround would be to do double reads, (ignoring side effects).

    Write cycles, as stated , are just fine.

    Thanks, Jure Z.

  • Jure Zaninovich said:
    on the read cycles, the processor drives the bus with stale data, data being correct for the previous access.

    What makes you think the processor is driving the bus with stale data?  For the case of a read my expectation is for the external device to do the driving of the bus.  Are you using the GPMC in a muxed or non-muxed mode?

  • we are capturing the data with chipscope ( Xilinx built in logic analyzer device probing the pins)

    yes we are configuring the GPMC in muxed mode as listed in earlier post:

     

    7.1.5.11 GPMC_CONFIG1_i

    9-8 MUXADDDATA : 2h Address and data multiplexed attached device

    Key: 

    0 Non-multiplexed attached device

    1h AAD-multiplexed protocol device

    2h Address and data multiplexed attached device

    3h Reserved

     

    I'll have to withdraw my statement  "the processor drives the data bus" , now that I think again, after you mentioned it.

    A better statement would be, " the data bus assumes the values that correspond to the previous read cycle".

    This clarification may lead into the posibility of something being wrong with the FPGA design itself...

     

     

    Thanks, Jure Z.

     

     

  • Jure Zaninovich said:

    I'll have to withdraw my statement  "the processor drives the data bus" , now that I think again, after you mentioned it.

    A better statement would be, " the data bus assumes the values that correspond to the previous read cycle".

    Aside from driving the address onto the pins, the processor would not be driving the bus.  It sounds to me like either you don't have the correct timing to talk to the FPGA or else something is wrong inside the FPGA itself.  If there is some kind of delay internal to the FPGA upon receiving the address you might need to implement a WAIT pin so the FPGA can temporarily stall the transfer until it has the data ready.