Anybody having any issues getting the DDR2 on AM335X to run reliably at 266MHz? On our first spin of boards that were using engineering samples of the AM335X I have an issue with DDR2 not running reliably above 240MHz. At 266MHz I have a memory test where I can get one bit to fail. The way I get it to fail is by flipping all the data bits from all 0's to all 1's ---- I will sometimes see a one bit error in this situation. I do not have the problem if I slow the DDR2 down to 240MHz. And yes I have used the TI spreadsheet tools to set up my DDR2. The Micron memory chip I am interfacing to is good to 400MHz.
Our next set of boards with fully qualified Industrial AM335X chips will arrive this coming week, so hopefully I can go back to full speed (266MHz DDR2) with these new boards.