Other Parts Discussed in Thread: DM385
Hi,
Although AM335X AES HW supports many modes, but the AES driver only supports CBC, ECB and CTR mode. Some customers want to use GCM mode. By looking at the driver, I see I need to do following changes in omap4-aes.c but I would like you review it, especailly for #4).
Thanks a lot.
Bin
1). Add an ALG in struct crypto_alg alg[ ] for "gcm(aes)" ;
2). Add
#define FLAGS_GCM BIT(7)
3). Add two functions:
static int omap4_aes_gcm_encrypt(struct ablkcipher_request *req)
{
return omap4_aes_crypt(req, FLAGS_ENCRYPT | FLAGS_GCM);
}
static int omap4_aes_gcm_decrypt(struct ablkcipher_request *req)
{
return omap4_aes_crypt(req, FLAGS_GCM);
}
4). Change omap4_aes_ctr_encrypt():
static int omap4_aes_write_ctrl(struct omap4_aes_dev *dd)
{
unsigned int key32;
int i, err;
u32 val, mask;
err = omap4_aes_hw_init(dd);
if (err)
return err;
pr_debug("Set key\n");
key32 = dd->ctx->keylen / sizeof(u32);
/* set a key */
for (i = 0; i < key32; i++) {
omap4_aes_write(dd, AES_REG_KEY1(i),
__le32_to_cpu(dd->ctx->key[i]));
}
if ((dd->flags & (FLAGS_CBC | FLAGS_CTR | FLAGS_GCM)) && dd->req->info)
omap4_aes_write_n(dd, AES_REG_IV(0), dd->req->info, 4);
val = FLD_VAL(((dd->ctx->keylen >> 3) - 1), 4, 3);
if (dd->flags & FLAGS_CBC)
val |= AES_REG_CTRL_CBC;
else if (dd->flags & FLAGS_CTR)
val |= AES_REG_CTRL_CTR | AES_REG_CTRL_CTR_WIDTH_32;
else if (dd->flags & FLAGS_GCM)
val |= AES_REG_CTRL_GCM | AES_REG_CTRL_CTR | AES_REG_CTRL_CTR_WIDTH_32;
<-- This is the part I'm not sure: are we always using Autonomous GHASH? CTRL_CTR also needs to be set for GCM, right? Is WIDTH_32 right value for GCM?
if (dd->flags & FLAGS_ENCRYPT)
val |= AES_REG_CTRL_DIRECTION;
mask = AES_REG_CTRL_CBC | AES_REG_CTRL_CTR | AES_REG_CTRL_GCM | AES_REG_CTRL_DIRECTION |
AES_REG_CTRL_KEY_SIZE_MASK | AES_REG_CTRL_CTR_WIDTH_MASK;
omap4_aes_write_mask(dd, AES_REG_CTRL, val, mask);
return 0;
}