Other Parts Discussed in Thread: TPS65217, AM3354
Hello,
Can someone please let me know if there is a discrepancy in the TRM for the Core PLL table 655. If one considers the clock_am335x.h, the COREPLL_M is set to 1000 which results into a 2Ghz clock, this matches the datasheet.
But the datasheet value for COREPLL_M6 does not match the definition in the header file. The header file definition seems correct.
Can someone please confirm the same.
Also based on the datasheet, in order for me to allow 275Mhz operation for the MPU I only need to define COREPLL_M to 275. Is that correct? (I"m using the 27 speed grade part on the ZCE so the max frequency for the MPU is 275Mhz)
Thank you for your replies
Regards
Santhosh