I have strange problem with my watchdog on AM3505. Working with omap_wdt driver, took the wdt application from kernel documentation. Using 2.6.37.
Seems that when the kernel was sometimes blocked (on other problems I've had), the watchdog was resetting the system.
Unfortunately, I am unable to do the reset triggering manually. I am running my keep alive while routine application in background. Then I kill it and wait for the preset timeout but no reboot occurs.
Later, I have added in omap_wdt_open() the following lines, to ensure the interrupt is generated on overflow (since no stall condition is issued in my case):
// Should generate interrupt on overflow
+#define OMAP_WATCHDOG_WISR (0x18)
+#define OMAP_WATCHDOG_WIER (0x1C)
+__raw_writel(0x1, (base + OMAP_WATCHDOG_WIER));
+__raw_writel(0x1, (base + OMAP_WATCHDOG_WISR));
+__raw_writel(0x2B, (base + OMAP_WATCHDOG_SYS_CONFIG));
But it still doesn't help.
...
Another interesting exercise. When I am building my watchdog app with a while loop patting the dog and actually removing the call for the wdt keep-alive func inside, then booting and running it in background - reboot happens exactly after the preconf. timeout!
Please advise,
Regards
Yakir
PS. My omap_wdt driver file attached
/*
* omap_wdt.c
*
* Watchdog driver for the TI OMAP 16xx & 24xx/34xx 32KHz (non-secure) watchdog
*
* Author: MontaVista Software, Inc.
* <gdavis@mvista.com> or <source@mvista.com>
*
* 2003 (c) MontaVista Software, Inc. This file is licensed under the
* terms of the GNU General Public License version 2. This program is
* licensed "as is" without any warranty of any kind, whether express
* or implied.
*
* History:
*
* 20030527: George G. Davis <gdavis@mvista.com>
* Initially based on linux-2.4.19-rmk7-pxa1/drivers/char/sa1100_wdt.c
* (c) Copyright 2000 Oleg Drokin <green@crimea.edu>
* Based on SoftDog driver by Alan Cox <alan@lxorguk.ukuu.org.uk>
*
* Copyright (c) 2004 Texas Instruments.
* 1. Modified to support OMAP1610 32-KHz watchdog timer
* 2. Ported to 2.6 kernel
*
* Copyright (c) 2005 David Brownell
* Use the driver model and standard identifiers; handle bigger timeouts.
*/
#include <linux/module.h>
#include <linux/types.h>
#include <linux/kernel.h>
#include <linux/fs.h>
#include <linux/mm.h>
#include <linux/miscdevice.h>
#include <linux/watchdog.h>
#include <linux/reboot.h>
#include <linux/init.h>
#include <linux/err.h>
#include <linux/platform_device.h>
#include <linux/moduleparam.h>
#include <linux/bitops.h>
#include <linux/io.h>
#include <linux/uaccess.h>
#include <linux/slab.h>
#include <linux/pm_runtime.h>
#include <mach/hardware.h>
#include <plat/prcm.h>
#include "omap_wdt.h"
static struct platform_device *omap_wdt_dev;
static unsigned timer_margin;
module_param(timer_margin, uint, 0);
MODULE_PARM_DESC(timer_margin, "initial watchdog timeout (in seconds)");
static unsigned int wdt_trgr_pattern = 0x1234;
static spinlock_t wdt_lock;
struct omap_wdt_dev {
void __iomem *base; /* physical */
struct device *dev;
int omap_wdt_users;
struct resource *mem;
struct miscdevice omap_wdt_miscdev;
};
static void omap_wdt_ping(struct omap_wdt_dev *wdev)
{
void __iomem *base = wdev->base;
/* wait for posted write to complete */
while ((__raw_readl(base + OMAP_WATCHDOG_WPS)) & 0x08)
cpu_relax();
wdt_trgr_pattern = ~wdt_trgr_pattern;
__raw_writel(wdt_trgr_pattern, (base + OMAP_WATCHDOG_TGR));
/* wait for posted write to complete */
while ((__raw_readl(base + OMAP_WATCHDOG_WPS)) & 0x08)
cpu_relax();
/* reloaded WCRR from WLDR */
}
static void omap_wdt_enable(struct omap_wdt_dev *wdev)
{
void __iomem *base = wdev->base;
/* Sequence to enable the watchdog */
__raw_writel(0xBBBB, base + OMAP_WATCHDOG_SPR);
while ((__raw_readl(base + OMAP_WATCHDOG_WPS)) & 0x10)
cpu_relax();
__raw_writel(0x4444, base + OMAP_WATCHDOG_SPR);
while ((__raw_readl(base + OMAP_WATCHDOG_WPS)) & 0x10)
cpu_relax();
}
static void omap_wdt_disable(struct omap_wdt_dev *wdev)
{
void __iomem *base = wdev->base;
/* sequence required to disable watchdog */
__raw_writel(0xAAAA, base + OMAP_WATCHDOG_SPR); /* TIMER_MODE */
while (__raw_readl(base + OMAP_WATCHDOG_WPS) & 0x10)
cpu_relax();
__raw_writel(0x5555, base + OMAP_WATCHDOG_SPR); /* TIMER_MODE */
while (__raw_readl(base + OMAP_WATCHDOG_WPS) & 0x10)
cpu_relax();
}
static void omap_wdt_adjust_timeout(unsigned new_timeout)
{
if (new_timeout < TIMER_MARGIN_MIN)
new_timeout = TIMER_MARGIN_DEFAULT;
if (new_timeout > TIMER_MARGIN_MAX)
new_timeout = TIMER_MARGIN_MAX;
timer_margin = new_timeout;
}
static void omap_wdt_set_timeout(struct omap_wdt_dev *wdev)
{
u32 pre_margin = GET_WLDR_VAL(timer_margin);
void __iomem *base = wdev->base;
/* just count up at 32 KHz */
while (__raw_readl(base + OMAP_WATCHDOG_WPS) & 0x04)
cpu_relax();
__raw_writel(pre_margin, base + OMAP_WATCHDOG_LDR);
while (__raw_readl(base + OMAP_WATCHDOG_WPS) & 0x04)
cpu_relax();
}
/*
* Allow only one task to hold it open
*/
static int omap_wdt_open(struct inode *inode, struct file *file)
{
struct omap_wdt_dev *wdev = platform_get_drvdata(omap_wdt_dev);
void __iomem *base = wdev->base;
if (test_and_set_bit(1, (unsigned long *)&(wdev->omap_wdt_users)))
return -EBUSY;
pm_runtime_get_sync(wdev->dev);
/* initialize prescaler */
while (__raw_readl(base + OMAP_WATCHDOG_WPS) & 0x01)
cpu_relax();
__raw_writel((1 << 5) | (PTV << 2), base + OMAP_WATCHDOG_CNTRL);
while (__raw_readl(base + OMAP_WATCHDOG_WPS) & 0x01)
cpu_relax();
file->private_data = (void *) wdev;
omap_wdt_set_timeout(wdev);
omap_wdt_ping(wdev); /* trigger loading of new timeout value */
omap_wdt_enable(wdev);
// Should generate interrupt on overflow
__raw_writel(0x1, (base + OMAP_WATCHDOG_WIER));
__raw_writel(0x1, (base + OMAP_WATCHDOG_WISR));
__raw_writel(0x2B, (base + OMAP_WATCHDOG_SYS_CONFIG));
return nonseekable_open(inode, file);
}
static int omap_wdt_release(struct inode *inode, struct file *file)
{
struct omap_wdt_dev *wdev = file->private_data;
/*
* Shut off the timer unless NOWAYOUT is defined.
*/
#ifndef CONFIG_WATCHDOG_NOWAYOUT
omap_wdt_disable(wdev);
pm_runtime_put_sync(wdev->dev);
#else
printk(KERN_CRIT "omap_wdt: Unexpected close, not stopping!\n");
#endif
wdev->omap_wdt_users = 0;
return 0;
}
static ssize_t omap_wdt_write(struct file *file, const char __user *data,
size_t len, loff_t *ppos)
{
struct omap_wdt_dev *wdev = file->private_data;
/* Refresh LOAD_TIME. */
if (len) {
spin_lock(&wdt_lock);
omap_wdt_ping(wdev);
spin_unlock(&wdt_lock);
}
return len;
}
static long omap_wdt_ioctl(struct file *file, unsigned int cmd,
unsigned long arg)
{
struct omap_wdt_dev *wdev = platform_get_drvdata(omap_wdt_dev);
int new_margin;
static const struct watchdog_info ident = {
.identity = "OMAP Watchdog",
.options = WDIOF_SETTIMEOUT,
.firmware_version = 0,
};
wdev = file->private_data;
switch (cmd) {
case WDIOC_GETSUPPORT:
return copy_to_user((struct watchdog_info __user *)arg, &ident,
sizeof(ident));
case WDIOC_GETSTATUS:
return put_user(0, (int __user *)arg);
case WDIOC_GETBOOTSTATUS:
if (cpu_is_omap16xx())
return put_user(__raw_readw(ARM_SYSST),
(int __user *)arg);
if (cpu_is_omap24xx())
return put_user(omap_prcm_get_reset_sources(),
(int __user *)arg);
case WDIOC_KEEPALIVE:
spin_lock(&wdt_lock);
omap_wdt_ping(wdev);
spin_unlock(&wdt_lock);
return 0;
case WDIOC_SETTIMEOUT:
if (get_user(new_margin, (int __user *)arg))
return -EFAULT;
omap_wdt_adjust_timeout(new_margin);
spin_lock(&wdt_lock);
omap_wdt_disable(wdev);
omap_wdt_set_timeout(wdev);
omap_wdt_enable(wdev);
omap_wdt_ping(wdev);
spin_unlock(&wdt_lock);
/* Fall */
case WDIOC_GETTIMEOUT:
return put_user(timer_margin, (int __user *)arg);
default:
return -ENOTTY;
}
}
static const struct file_operations omap_wdt_fops = {
.owner = THIS_MODULE,
.write = omap_wdt_write,
.unlocked_ioctl = omap_wdt_ioctl,
.open = omap_wdt_open,
.release = omap_wdt_release,
.llseek = no_llseek,
};
static int __devinit omap_wdt_probe(struct platform_device *pdev)
{
struct resource *res, *mem;
struct omap_wdt_dev *wdev;
int ret;
/* reserve static register mappings */
res = platform_get_resource(pdev, IORESOURCE_MEM, 0);
if (!res) {
ret = -ENOENT;
goto err_get_resource;
}
if (omap_wdt_dev) {
ret = -EBUSY;
goto err_busy;
}
mem = request_mem_region(res->start, resource_size(res), pdev->name);
if (!mem) {
ret = -EBUSY;
goto err_busy;
}
wdev = kzalloc(sizeof(struct omap_wdt_dev), GFP_KERNEL);
if (!wdev) {
ret = -ENOMEM;
goto err_kzalloc;
}
wdev->omap_wdt_users = 0;
wdev->mem = mem;
wdev->dev = &pdev->dev;
wdev->base = ioremap(res->start, resource_size(res));
if (!wdev->base) {
ret = -ENOMEM;
goto err_ioremap;
}
platform_set_drvdata(pdev, wdev);
pm_runtime_enable(wdev->dev);
pm_runtime_get_sync(wdev->dev);
omap_wdt_disable(wdev);
omap_wdt_adjust_timeout(timer_margin);
wdev->omap_wdt_miscdev.parent = &pdev->dev;
wdev->omap_wdt_miscdev.minor = WATCHDOG_MINOR;
wdev->omap_wdt_miscdev.name = "watchdog";
wdev->omap_wdt_miscdev.fops = &omap_wdt_fops;
ret = misc_register(&(wdev->omap_wdt_miscdev));
if (ret)
goto err_misc;
pr_info("OMAP Watchdog Timer Rev 0x%02x: initial timeout %d sec\n",
__raw_readl(wdev->base + OMAP_WATCHDOG_REV) & 0xFF,
timer_margin);
pm_runtime_put_sync(wdev->dev);
omap_wdt_dev = pdev;
return 0;
err_misc:
platform_set_drvdata(pdev, NULL);
iounmap(wdev->base);
err_ioremap:
wdev->base = NULL;
kfree(wdev);
err_kzalloc:
release_mem_region(res->start, resource_size(res));
err_busy:
err_get_resource:
return ret;
}
static void omap_wdt_shutdown(struct platform_device *pdev)
{
struct omap_wdt_dev *wdev = platform_get_drvdata(pdev);
if (wdev->omap_wdt_users)
omap_wdt_disable(wdev);
}
static int __devexit omap_wdt_remove(struct platform_device *pdev)
{
struct omap_wdt_dev *wdev = platform_get_drvdata(pdev);
struct resource *res = platform_get_resource(pdev, IORESOURCE_MEM, 0);
if (!res)
return -ENOENT;
misc_deregister(&(wdev->omap_wdt_miscdev));
release_mem_region(res->start, resource_size(res));
platform_set_drvdata(pdev, NULL);
iounmap(wdev->base);
kfree(wdev);
omap_wdt_dev = NULL;
return 0;
}
#ifdef CONFIG_PM
/* REVISIT ... not clear this is the best way to handle system suspend; and
* it's very inappropriate for selective device suspend (e.g. suspending this
* through sysfs rather than by stopping the watchdog daemon). Also, this
* may not play well enough with NOWAYOUT...
*/
static int omap_wdt_suspend(struct platform_device *pdev, pm_message_t state)
{
struct omap_wdt_dev *wdev = platform_get_drvdata(pdev);
if (wdev->omap_wdt_users)
omap_wdt_disable(wdev);
return 0;
}
static int omap_wdt_resume(struct platform_device *pdev)
{
struct omap_wdt_dev *wdev = platform_get_drvdata(pdev);
if (wdev->omap_wdt_users) {
omap_wdt_enable(wdev);
omap_wdt_ping(wdev);
}
return 0;
}
#else
#define omap_wdt_suspend NULL
#define omap_wdt_resume NULL
#endif
static struct platform_driver omap_wdt_driver = {
.probe = omap_wdt_probe,
.remove = __devexit_p(omap_wdt_remove),
.shutdown = omap_wdt_shutdown,
.suspend = omap_wdt_suspend,
.resume = omap_wdt_resume,
.driver = {
.owner = THIS_MODULE,
.name = "omap_wdt",
},
};
static int __init omap_wdt_init(void)
{
spin_lock_init(&wdt_lock);
return platform_driver_register(&omap_wdt_driver);
}
static void __exit omap_wdt_exit(void)
{
platform_driver_unregister(&omap_wdt_driver);
}
module_init(omap_wdt_init);
module_exit(omap_wdt_exit);
MODULE_AUTHOR("George G. Davis");
MODULE_LICENSE("GPL");
MODULE_ALIAS_MISCDEV(WATCHDOG_MINOR);
MODULE_ALIAS("platform:omap_wdt");
My wdt app code:
#include <linux/types.h>
#include <linux/watchdog.h>
#include <mmx_defs.h>
#include <err_codes.h>
#define DEFAULT_TO 60
#define DEFAULT_PRE_TO 5
int fd, timeout, pre_timeout = DEFAULT_PRE_TO;
/*
* This function simply sends an IOCTL to the driver, which in turn ticks
* the PC Watchdog card to reset its internal timer so it doesn't trigger
* a computer reset.
*/
static void keep_alive(void)
{
int dummy;
ioctl(fd, WDIOC_KEEPALIVE, &dummy);
}
/* The main program. Run the program with "-d" to disable the card,
* or "-e" to enable the card.
*/
int main(int argc, char *argv[])
{
int flags;
fd = open("/dev/watchdog", O_WRONLY);
if (-1 == fd)
{
PRINT_STDERR("Error! WDT device is not enabled or in use!\n");
fflush(stderr);
exit(-1);
}
if (argc > 1)
{
if (!strncasecmp(argv[1], "-d", 2))
{
flags = WDIOS_DISABLECARD;
ioctl(fd, WDIOC_SETOPTIONS, &flags);
fprintf(stderr, "WDT is disabled.\n");
fflush(stderr);
close(fd);
exit(0);
}
else if (!strncasecmp(argv[1], "-e", 2))
{
flags = WDIOS_ENABLECARD;
ioctl(fd, WDIOC_SETOPTIONS, &flags);
timeout = (NULL == argv[2]) ? DEFAULT_TO : atoi(argv[2]);
ioctl(fd, WDIOC_SETTIMEOUT, &timeout);
ioctl(fd, WDIOC_SETPRETIMEOUT, &pre_timeout);
fprintf(stderr, "WDT is enabled, timeout = %d[s], pre-timeout = %d[s]\n", timeout, pre_timeout);
fflush(stderr);
close(fd);
exit(0);
}
else
{
fprintf(stderr, "-d to disable, -e to enable.\n");
fprintf(stderr, "Run by itself to tick the timer.\n");
fflush(stderr);
close(fd);
exit(0);
}
}
else
{
fprintf(stderr, "WDT is ticking away...\n");
fflush(stderr);
}
// Watchdog Loop
while(1)
{
keep_alive();
sleep(5);
}
close(fd); //shouldn't get here, but it is a "good practice" action
}
I've disabled the NOWAYOUT option in the kernel