This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x SD card connection detect pin

Hello

      We are designing AM335x Android custom device based on AM335xevm_SK kit.

      We need to use UART3_rxd_mux1 on C15 ball. But AM335X_SPI0_CS1 (Connection detect pin ) connected with C15 ball.

      In board file (board-am335xevm.c)  SDcard connection detect pin configured as GPIO (gpio.0_6). 

     Can we connect SD connection detect pin to any GPIO or its need to connect with only C15?

Thanks

KUmar.