I am doing some tests using PRU assembly to figure out the architecture of PRU but I am very confused about memory map explained in the manual "AM335x PRU-ICSS Reference Guide" and here are the points. I know that TI does not support such information but maybe someone is willing to reply.
1. I am sending one char to the UART0 using the global address 0x44e0_9000 and it works fine. I am doing that using the OCP slave port.
2. I try to do the same using the local address 0x0002_8000 (table 5, page 19) without use the OCP slave but it doesn't work.
I don't understand based on the table 6 (Global memory map offset addresses) how to obtain the global address 0x44e0_9000, I have no idea how can I map 0x0002_8000 to 0x44e0_9000. I would like to know how to determine the local address based on global address.
Sincerely,
Jorge Ventura