Hello,
We try to configure GPIO pin as the open drain mode. But based on AM335x document, it looks like GPIO can't be configured as the open drain mode. Can you help me confirm if AM335x GPIO pin can be configured as as the open drain mode? And it looks like there are 2 i/o pin AIN3 and AIN4 available within the AM335x that have what appears to be open drain outputs. Can TI confirm if these pins would suffice electrically for us trying to accomplish with OneWire protocol.Note the onewire protocol based from the TI "application report SLAA196 - Feb 2004" titled "HDQ Protocol Implementation with MSP430".
Thanks,Jian