This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Confusion about I/O direction of SPI pins



On a custom hardware I use SPI1 to configure an LC display. The AM335x and the LCD are connected as follows:

AM335x -- LCD

SPI1_D0 -> SDI (input)
SPI1_D1 <- SDO (output)
SPI1_CLK -> CLK
SPI1_CS0 -> CS

I use spidev to transfer date from the AM335x to the LCD.

With the oscilloscope I can see that SPI1_CLK and SPI_CS0 are working perfectly. It is just the data output line (SPI1_D0) that does not change. No matter if configured it as input or output in the pinmux. By default (i.e. if I don't make any changes to 'omap2_mcspi_setup_transfer') SPI1_D0 is MOSI, SPI1_D1 is MISO and the SOC behaves like an SPI master, correct?

What am I doing wrong here?

many thanks and kind regards, Felix

  • Hi Felix,
     
    Besides input/output have you set your pins to SPI mode?
  • Hi Felix,

    Which processor pins are you using to mux the SPI1 signals?

    Please check if these pins are muxed correctly from user space:

    1. Mount the debugfs: mount -t debugfs none /sys/kernel/debug/
    2. Check the current pinmux configurations for your pins:
    cat /sys/kernel/debug/omap_mux/<pin_name>

    This should give you information about the current mux configuration for the pin.

    Best regards,
    Miroslav

  • Hello Miroslav,

    Thanks for this tip. When I enter 'cat /sys/kernel/debug/omap_mux/mcasp0_fsx' I get the following:

    name: mcasp0_fsx.spi1_d0 (0x44e10994/0x994 = 0x0003), b NA, t NA
    mode: OMAP_MUX_MODE3 | AM33XX_PIN_OUTPUT
    signals: mcasp0_fsx | NA | NA | spi1_d0 | mmc1_sdcd | NA | NA | gpio3_15

    Doesn't this look fine? According to this I would expect SPI1 data to be output on SPI1_D0.

    regards Felix

  • Hello Biser,

    I don't understand this. What do you mean by 'have you set your pins to SPI mode'? CS and CLK are working as expected.

    regards, Felix

  • It's OK. You already answered Miroslav and it seems correct muxmode is selected. One more thing - do you have rx enabled on the SPI clock pinmux register?
  • When I enter 'cat /sys/kernel/debug/omap_mux/mcasp0_aclkx' I get this:


    name: mcasp0_aclkx.spi1_sclk (0x44e10990/0x990 = 0x0023), b NA, t NA
    mode: OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLDOWN
    signals: mcasp0_aclkx | NA | NA | spi1_sclk | mmc0_sdcd | NA | NA | gpio3_14

    Looks fine to me. Just to make sure I explained correctly: the SOC is running as SPI master and do not see anything happen on pin SPI1_D0 which is supposed to output the serial data. CS and CLK are working.

  • For testing purposes I have configured SPI1_D0 to be be GPIO3_15. Setting it to output mode I can see on the oscilloscope that it toggles when I write 0/1 to it. At least I am sure now that the pin is working, i.e. it must be a wrong configuration in software.

    Looking at the 'board-am225xevm.c" file I can find for example the following pin configuration for SPI0:

    static struct pinmux_config spi0_pin_mux[] = {
        {"spi0_sclk.spi0_sclk", OMAP_MUX_MODE0 | AM33XX_PULL_ENBL
                                | AM33XX_INPUT_EN},
        {"spi0_d0.spi0_d0", OMAP_MUX_MODE0 | AM33XX_PULL_ENBL | AM33XX_PULL_UP
                                | AM33XX_INPUT_EN},
        {"spi0_d1.spi0_d1", OMAP_MUX_MODE0 | AM33XX_PULL_ENBL
                                | AM33XX_INPUT_EN},
        {"spi0_cs0.spi0_cs0", OMAP_MUX_MODE0 | AM33XX_PULL_ENBL | AM33XX_PULL_UP
                                | AM33XX_INPUT_EN},
        {NULL, 0},

    But how is this supposed to work? Who or what configures D0 or D1 to be MOSI (the output)?

    regards Felix

  • These would be the DPE1 and DPE0 bits in the MCSPI_CH[0:1]CONF register.
  • Hello Biser,

    I knew that but did somehow not fully realize. The TRM (version h) at 24.4.1.18 states that after reset DP0 is 0 and DPE1 is 1. My conclusion was that SPIDAT[0] gets selected as transmission line. So far this is correct, but in file 'spi-omap2-mcspi.c' theses settings get modified in function 'omap2_mcspi_setup_transfer':

        l &= ~(OMAP2_MCSPI_CHCONF_IS|OMAP2_MCSPI_CHCONF_DPE1);
        l |= OMAP2_MCSPI_CHCONF_DPE0;

    This was exactly my problem as this code 'reverts' the default settings of DPE0/1. After the following modification to the code my LC display finally accepts configuration commands from the SOC:

        l &= ~(OMAP2_MCSPI_CHCONF_IS|OMAP2_MCSPI_CHCONF_DPE0);
        l |= OMAP2_MCSPI_CHCONF_DPE1;

    Thank you very much for pushing me into the right direction, Felix

  • Just some additional information for those struggling with SPI data pin direction:

    Meanwhile I'm on kernel 4.5 using device tree. There is no more need to modify any code, just add the ti,pindir-d0-out-d1-in property to the corresponding SPI device. The property is described in the binding documentation found at ./Documentation/devicetree/bindings/spi/omap-spi.txt.

    My DTS file therefore contains the following code:

    &spi1 {
        pinctrl-names = "default";
        pinctrl-0 = <&spi1_pins>;
        ti,pindir-d0-out-d1-in;
        status = "okay";

        cfaf240320a032t {
            compatible = "crystalfontz,cfaf240320a032t";
            reg = <0>;
            spi-max-frequency = <1000000>;
            // SPI mode 3
            spi-cpol;
            spi-cpha;
            status = "okay";
        };
    };

    Et voilà, it works! Hope this might help somebody, Felix