Other Parts Discussed in Thread: TLK110, TLK105, TLK106
Our customer is not using a default PHY, i.e. TLK105, TLK106 and TLK110.
The MII in PRU-ICSS has the pr1_mii0_rxlink and the pr1_mii1_rxlink for the LINK_MII signal. This signal used for link detection connects to typically an LED output signal of the PHY.
If the PHY does not have those signals, the LINK_MII signal is unavailable. If so, reading out MII management interface registers instead of using a dedicated link signal is needed.
Does the PRU with current version of Industrial SDK support the other operation for link detection instead of using a dedicated link signal?
Best regards,
Daisuke