Other Parts Discussed in Thread: AM3354, TPS65910, TPS65217, AM3358
Now I porting the am335x sdk ti-sdk-am335x-evm-06.00.00.00 to a customer board
When bring up the board ,there is a warning in the kernel log
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0 (root@Vm-ubuntu) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #67 Thu Nov 21 17:23:15 CST 2013
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES1.0 (sgx neon )
[ 0.000000] ------------[ cut here ]------------
[ 0.000000] WARNING: at arch/arm/mach-omap2/clkt_clksel.c:194 omap2_clksel_recalc+0xc8/0x134()
[ 0.000000] clock: Could not find fieldval 0 for clock dpll_core_m6_ck parent dpll_core_x2_ck
[ 0.000000] Modules linked in:
[ 0.000000] Backtrace:
[ 0.000000] [<c0017dbc>] (dump_backtrace+0x0/0x10c) from [<c04113d4>] (dump_stack+0x18/0x1c)
[ 0.000000] r6:c0030b28 r5:00000009 r4:c05d1e78 r3:c05f308c
[ 0.000000] [<c04113bc>] (dump_stack+0x0/0x1c) from [<c003e610>] (warn_slowpath_common+0x54/0x6c)
[ 0.000000] [<c003e5bc>] (warn_slowpath_common+0x0/0x6c) from [<c003e6cc>] (warn_slowpath_fmt+0x38/0x40)
[ 0.000000] r8:80000200 r7:c064eaa4 r6:00000000 r5:c05e4c38 r4:00000000
[ 0.000000] r3:00000009
[ 0.000000] [<c003e694>] (warn_slowpath_fmt+0x0/0x40) from [<c0030b28>] (omap2_clksel_recalc+0xc8/0x134)
[ 0.000000] r3:00000000 r2:c04fe938
[ 0.000000] [<c0030a60>] (omap2_clksel_recalc+0x0/0x134) from [<c0034ba0>] (propagate_rate+0x34/0x54)
[ 0.000000] r6:c064eadc r5:c05e4b38 r4:c05e4c38
[ 0.000000] [<c0034b6c>] (propagate_rate+0x0/0x54) from [<c0034bac>] (propagate_rate+0x40/0x54)
Can anybody give me some suggestion?