This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

"AM3358BZCZ100" power supply.



 I have some questions about power design.

 Processor is "AM3358BZCZ100" and PMU is "TPS65910A3A1RSL" , using DDR3

We should provide different voltage to processor according to processor frequency

(1)I need your confirmation for "AM3358BZCZ100" power supply.

VDD_MPU : 1.325V      yes or no
VDD_CORE: 1.1V         yes or no

(2) I am not sure VDD_MPU is 1.1V is also meet requirements if using AM3358BZCZ100.

  • Hi Burt,

    Linux should handle this automatically depending on the operating frequency chosen. Just make sure you connect both I2C and SR pins of the PMIC to I2C0 of the processor.

  • Yes, I got.

    For PMIC the default value is 1.1V for VDD_MPU and VDDMPU when selecting EEPROM mode. your means is that is ok for processor AM3358BZCZ100 in spite of its work frequency is 1GHz. Why?

    I am not sure when power on processor  AM3358BZCZ100 it start working on lower frequency ,maybe it is 500Mhz, so, 1.1V core and MPU voltage are all ok for it.

    And later if it want to work on high frequency , it will handle PMIC through I2C, and change register and get different voltage and meet high frequency.

    Do you agree my understand? Could you give me explanation if I made mistake. Thanks

  • Yes, this is correct. The processor inits at MPU frequency 500MHz. Everything else is handled once the initial software is loaded and starts executing.