Other Parts Discussed in Thread: AM4377
Hello,
looking for a fast ethernet solution without using LINUX I came over the Industrial Software Development Kit (IDK)
which supports several industrial ethernet protocolls using the PRUSS.
I actually dont't need an industrial protocoll. Data shall be received and sent by a normal Windows7 PC. But I fancy
the idea of having communication run on a separate processor thus not interrupting other processes that run
simultaneously (data collection mainly).
From that the following questions arise:
1. Which communication protocoll (that runs on the PRUSS) provided by the IDK can be used to communicate with a
normal PC, i.e. via a standard ethernet connection?
2. Is UDP supported?
3. Are both PRUSSs used for ethernet communication? Or is one PRUSS left for other purposes?
Does anybody know?
Thank you?
Martin