Other Parts Discussed in Thread: AM3359
hello,
I try to run the mcasp0 on my custom am3359 board with a the max9860 codec, according to the debug message the mcasp0 seems to be well initialized (see above), but when i try to play sound with aplay, the "aplay" command there is no signal on the mcasp0 pins and the aplay command not exit, to do it, i must use ctrl+c key.
i try to change instance number of the mcasp0 to 1 (see above) in the function but no change.
static struct snd_soc_dai_link am335x_evm_sk_dai = {
.cpu_dai_name = "davinci-mcasp.0", //replace by 1
};
/* Setup McASP 0 */
static void mcasp0_init(int evm_id, int profile)
{
am335x_register_mcasp(&am335x_P0519_snd_data0, 0); //replace by 1
my config is that :
static u8 am335x_P0519_iis_serializer_direction1[] = {
TX_MODE, RX_MODE, INACTIVE_MODE, INACTIVE_MODE, //AXR0 en transmission et AXR1 en reception et les autres inactifs
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
};
static struct snd_platform_data am335x_P0519_snd_data0 = {
.tx_dma_offset = 0x46000000, /* McASP0 */
.rx_dma_offset = 0x46000000,
.op_mode = DAVINCI_MCASP_IIS_MODE,
.num_serializer = ARRAY_SIZE(am335x_P0519_iis_serializer_direction1),
.tdm_slots = 2, //mode I2S = 2 slots left and right
.serial_dir = am335x_P0519_iis_serializer_direction1,
.asp_chan_q = EVENTQ_2,
.version = MCASP_VERSION_3,
.txnumevt = 32,//taille de la FIFO pour les events
.rxnumevt = 32,//taille de la FIFO pour les events
.get_context_loss_count =
omap_pm_get_dev_context_loss_count,
};
static struct snd_soc_dai_link am335x_evm_sk_dai = {
.name = "MAX9860",
.stream_name = "Playback",
.cpu_dai_name = "davinci-mcasp.0",
.codec_dai_name = "max9860-hifi",
.codec_name = "max9860-codec.1-0010",
.platform_name = "davinci-pcm-audio",
.ops = &evm_ops,
};
/* Setup McASP 0 */
static void mcasp0_init(int evm_id, int profile)
{
/* Configure McASP */
setup_pin_mux(mcasp0_pin_mux);
am335x_register_mcasp(&am335x_P0519_snd_data0, 0);
return;
}
/* Module pin mux for mcasp0 pour la gestion de l'audio*/
static struct pinmux_config mcasp0_pin_mux[] = {
{"mcasp0_aclkx.mcasp0_aclkx", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT}, //BCLK en sortie
{"mcasp0_fsx.mcasp0_fsx", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT}, //FRAME sync en sortie
{"mcasp0_axr1.mcasp0_axr1", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLDOWN}, //AXR1 en entrée série synchrone
{"mcasp0_axr0.mcasp0_axr0", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT}, //AXR0 en sortie série synchrone
{"mcasp0_ahclkr.mcasp0_ahclkr", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT}, //non utilisé sortie horloge serie réception
{"mcasp0_aclkr.mcasp0_aclkr", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT}, //non utilisé sortie horloge serie réception
{"mcasp0_fsr.mcasp0_fsr", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT}, //non utilisé FRAME sync réception en sortie
{"mcasp0_ahclkx.mcasp0_ahclkx", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT}, //non utilisé BCLK en sortie
{NULL, 0},
};
debug message :
Registered platform 'snd-soc-dummy'
[ 5.989959] init max9860
[ 5.992675] max9860-codec 1-0010: codec register 1-0010
[ 5.992706] max9860-codec 1-0010: dai register 1-0010 #1
[ 5.992706] Registered DAI 'max9860-hifi'
[ 5.992706] Registered codec 'max9860-codec.1-0010'
[ 6.008209] davinci-pcm-audio davinci-pcm-audio: platform register davinci-pcm-audio
[ 6.008239] Registered platform 'davinci-pcm-audio'
[ 6.008544] davinci-mcasp davinci-mcasp.0: dai register davinci-mcasp.0
[ 6.008575] Registered DAI 'davinci-mcasp.0'
[ 6.009094] soc-audio soc-audio.0: binding MAX9860 at idx 0
[ 6.009185] soc-audio soc-audio.0: probe AM335X EVM dai link 0 late -2
[ 6.009216] soc-audio soc-audio.0: probe AM335X EVM dai link 0 late -1
[ 6.009216] soc-audio soc-audio.0: probe AM335X EVM dai link 0 late 0
[ 6.009246] max9860 probe codec
[ 6.018402] soc-audio soc-audio.0: probe AM335X EVM dai link 0 late 1
[ 6.018432] soc-audio soc-audio.0: probe AM335X EVM dai link 0 late 2
[ 6.018493] max9860-codec 1-0010: read 2 => 0
[ 6.018524] max9860-codec 1-0010: read 10 => 0
[ 6.018524] max9860-codec 1-0010: read 10 => 0
[ 6.018554] max9860-codec 1-0010: read 10 => 0
[ 6.018554] max9860-codec 1-0010: read 10 => 0
[ 6.018676] max9860-codec 1-0010: read 10 => 0
[ 6.018676] max9860-codec 1-0010: write 10 = 80
[ 6.019104] max9860-codec 1-0010: read 10 => 80
[ 6.019104] max9860-codec 1-0010: write 10 = 88
[ 6.019439] max9860-codec 1-0010: read 2 => 0
[ 6.019470] max9860-codec 1-0010: write 2 = 4
[ 6.019805] max9860-codec 1-0010: read 10 => 88
[ 6.019805] max9860-codec 1-0010: write 10 = 8b
[ 6.020843] asoc: max9860-hifi <-> davinci-mcasp.0 mapping ok
[ 6.028289] soc-audio soc-audio.0: Registered card 'AM335X EVM'
[ 6.028320] ALSA device list:
[ 6.031433] #0: AM335X EVM
My codec is well registered :
root@am335x-evm:/usr/share/sounds/alsa# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: EVM [AM335X EVM], device 0: Playback max9860-hifi-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0