I am porting the u-boot-2014.10 to am335x.
Now, the code can run to _main in MLO stage.
The following is the code of function _main:
ENTRY(_main) /* * Set up initial C runtime environment and call board_init_f(0). */ #if defined(CONFIG_SPL_BUILD) && defined(CONFIG_SPL_STACK) ldr sp, =(CONFIG_SPL_STACK) #else ldr sp, =(CONFIG_SYS_INIT_SP_ADDR) #endif bic sp, sp, #7 /* 8-byte alignment for ABI compliance */ mov r2, sp sub sp, sp, #GD_SIZE /* allocate one GD above SP */ bic sp, sp, #7 /* 8-byte alignment for ABI compliance */ mov r9, sp /* GD is above SP */ mov r1, sp mov r0, #0 clr_gd: cmp r1, r2 /* while not at end of GD */ strlo r0, [r1] /* clear 32-bit GD word */ addlo r1, r1, #4 /* move to next */ blo clr_gd #if defined(CONFIG_SYS_MALLOC_F_LEN) && !defined(CONFIG_SPL_BUILD) sub sp, sp, #CONFIG_SYS_MALLOC_F_LEN str sp, [r9, #GD_MALLOC_BASE] #endif /* mov r0, #0 not needed due to above code */ bl board_init_f
------------------------------------------------------------------------------------
If insert a debug function at the beginning of _main, I can get the log message.
If insert the same debug function after "ldr sp, =(CONFIG_SPL_STACK)", the am335x will be halt.
I have test the whole DDR3, it has been working normally.
The following is the debug function:
void test_tag()
{
puts("here\n");
}
If I insert a loop at the beginning of the _main, I can get debug messages continuously.
Now, I don't know how to resolve the problem.
Can you help me? Thank you.