Other Parts Discussed in Thread: AM3358
Hi expert,
I am checking temperature sensor which is implemented in AM335x.
According to following wiki site, the sensor can measure temperature from -50 degree to 150 degree w/ 8-bit ADC.
http://processors.wiki.ti.com/index.php/AM335x_Thermal_Considerations
(Please see "Measuring Case Temperature")
Could you please confirm following questions about above 8-bit ADC and give me feedback ?
Q1. According to above wiki site,
"8-bit ADC gives the sensor a poor accuracy of ±10.8°C."
Is mentioned above correct information ? Is it mistake of "±1.08°C" ?
If "±10.8°C" is true, when user set thermal shutdown, is the range which thermal shutdown event will occur from 136.2°C to 157.8°C ?
Q2. Could you show me the table which is desribed about relation b/w ADC code and temperature ?
Best Regards,
Machida