Other Parts Discussed in Thread: AM3354
Hi everyone,
I tested the frequency of gpio of am3354, and the mpu clock is set to 720MHz, and CORE_CLKOUTM4 is set to 200MHz. I output 1 and 0 from GP1_16 like below:
*pSOC_GPIO_1_REGS_SET = 0x10000;
*pSOC_GPIO_1_REGS_CLR = 0x10000;
However, the frequency of the signal present at gpio pin can only achive almost 3MHz, i don't know why? Is the gpio have the ability to achive a frequency as higher as 20MHz?
Regards,
Huang.