Other Parts Discussed in Thread: DA8XX
NHD-4.3-480272MF-ATXI-T-1.pdfTFC-A9700RTWV35TR-02A REV 3.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DA8XX
NHD-4.3-480272MF-ATXI-T-1.pdfTFC-A9700RTWV35TR-02A REV 3.pdf
AM335X LCD Driver IC Circuitry:
This is my configuration for TPS6108DRC, the circuitry allows for multiple configurations using zero ohm resistors as jumpers. The output should be 22-24V and provide as much as 120mA current assuming that R259 is DNI (not populated) and R262 is DNI (not populated) and R63 is DNI (not popluated).
Using the AM335X + SK3358 Diagnostic Test v3.3:
The current configuration is sufficient to power the LCD, however when testing the LCD using the diagnostic tool and option number 9 (LCD), the screen updates and shows the gradient, color spectrum and a few other things. When I choose option 10 (Touch screen) the test fails. However the screen does register my touches in the corners. The issue I am seeing is that the screen is segmented, this tells me that the driver information is not correct. Can you please confirm this? Below are a few images of the screen during the LCD test (option number 9).
Attempting to follow the build process outlined by TI (see previous post for URL):
The following files were modified for my custom screen (datasheet provided in original post):
1. da8xx-fb.c
2. board-am335xevm.c
The following was added in da8xx-fb.c
This was added under the static struct da8xx_panel known_lcd_panels[]
/* ThreeFive TFC_A9700RTWV35TR_02 */
[4] = {
.name = "TFC_A9700RTWV35R_02",
.width = 800,
.height = 480,
.hfp = 40,
.hbp = 40,
.hsw = 48,
.vfp = 13,
.vbp = 13,
.vsw = 3,
.pxl_clk = 30000000
.invert_pxl_clk = 0,
};
The following was modified in board-am335xemv.c
static const struct display_panel disp_panel = {
WVGA,
24,
24,
COLOR_ACTIVE,
};
Continuing on after the file modification for the compilation process:
Step 1: make CROSS_COMPILE=arm-eabi- distclean
Output: awk '(NF && $1 !~ /^#/) { print $1 ": " $1 "_config; $(MAKE)" }' boards.cfg > .boards.depend
Step 2: make CROSS_COMPILE=arm-eabi-am335x_evm_config
Output: awk '(NF && $1 !~ /^#/) { print $1 ": " $1 "_config; $(MAKE)" }' boards.cfg > .boards.depend
Configuring for am335x_evm board...
Step 3: make CROSS_COMPILE=arm-eabi-
Output: /bin/bash: arm-eabi-gcc: command not found
/bin/bash: arm-eabi-gcc: command not found
dirname: missing operand
Try 'dirname --help' for more information.
Generating include/autoconf.mk
/bin/bash: line 3: arm-eabi-gcc: command not found
/bin/bash: arm-eabi-gcc: command not found
dirname: missing operand
Try 'dirname --help' for more information.
Generating include/autoconf.mk.dep
/bin/bash: line 3: arm-eabi-gcc: command not found
/bin/bash: arm-eabi-gcc: command not found
/bin/bash: arm-eabi-gcc: command not found
dirname: missing operand
Try 'dirname --help' for more information.
/bin/bash: arm-eabi-gcc: command not found
/bin/bash: arm-eabi-ld: command not found
/bin/bash: arm-eabi-gcc: command not found
dirname: missing operand
Try 'dirname --help' for more information.
/bin/bash: arm-eabi-gcc: command not found
dirname: missing operand
Try 'dirname --help' for more information.
arm-eabi-gcc -DDO_DEPS_ONLY \
-g -Os -fno-common -ffixed-r8 -msoft-float -D__KERNEL__ -I/home/nathan/rowboat-android/TI-Android-ICS-4.0.3_AM335x_3.0.1/u-boot/include -fno-builtin -ffreestanding -nostdinc -isystem -pipe -DCONFIG_ARM -D__ARM__ -march=armv5 -Wall -Wstrict-prototypes \
-o lib/asm-offsets.s lib/asm-offsets.c -c -S
/bin/bash: arm-eabi-gcc: command not found
Makefile:529: recipe for target 'lib/asm-offsets.s' failed
make: *** [lib/asm-offsets.s] Error 127
PROCESS FAILED.