Other Parts Discussed in Thread: AM3354
I'm using a custom board based heavily on the AM335x EVM but with a AM3354 device. I'm trying to add a device to my board on I2C-1, (currently I only have devices on I2C-0). When I run a check for devices on I2C-1 I get errors in u-boot:
U-Boot# i2c dev 1
Setting bus to 1
U-Boot# i2c probe
Valid chip addresses:i2c_probe: pads on bus 1 probably not configured (status=0x10)
i2c_probe: pads on bus 1 probably not configured (status=0x10)
i2c_probe: pads on bus 1 probably not configured (status=0x10)
i2c_probe: pads on bus 1 probably not configured (status=0x10)
And in the kernel:
[root /]# i2cdetect -y -r 1
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: [ 1188.831062] omap_i2c 4802a000.i2c: controller timed out
-- [ 1189.831029] omap_i2c 4802a000.i2c: controller timed out
-- [ 1190.851032] omap_i2c 4802a000.i2c: controller timed out
...
...
70: [ 1299.991028] omap_i2c 4802a000.i2c: controller timed out
-- [ 1301.011026] omap_i2c 4802a000.i2c: controller timed out
-- [ 1302.031024] omap_i2c 4802a000.i2c: controller timed out
-- [ 1303.051030] omap_i2c 4802a000.i2c: controller timed out
-- [ 1304.071025] omap_i2c 4802a000.i2c: controller timed out
-- [ 1305.091028] omap_i2c 4802a000.i2c: controller timed out
-- [ 1306.111024] omap_i2c 4802a000.i2c: controller timed out
-- [ 1307.131027] omap_i2c 4802a000.i2c: controller timed out
--
I guess I'm missing something when it comes to enabling a second I2C bus. I didn't make any bootloader changes, so I'm not surprised the bootloader commands failed to work, but I would have thought the kernel could have worked independently. I added the configuration of the I2C1 pins in the device tree:
i2c1_pins: pinmux_i2c1_pins {
pinctrl-single,pins = <
0x168 (PIN_INPUT | MUX_MODE3) /* uart0_ctsn.i2c1_sda */
0x16c (PIN_INPUT | MUX_MODE3) /* uart0_rtsn.i2c1_scl */
0x1A0 (PIN_INPUT | MUX_MODE7) /* mcasp0_aclkr.mcasp0_axr2 */
0x060 (PIN_INPUT | MUX_MODE7) /* gpmc_a8.mcasp0_aclkx */
0x064 (PIN_INPUT | MUX_MODE7) /* gpmc_a9.mcasp0_fsx */
>;
};
And I also "enabled" the I2C-1 bus by setting the status to ok:
i2c1: i2c@4802a000 {
pinctrl-names = "default";
pinctrl-0 = <&i2c1_pins>;
status = "okay";
clock-frequency = <200000>; /* 400KHz is our max, 100KHz is the processor min */
crtouch: crtouch@49 {
reg = <0x49>;
};
};
Despite these changes it seems that there's more to be done. Can someone point me in the right direction for enabling I2C-1 please? (both in the bootloader and kernel would be helpful)