Other Parts Discussed in Thread: SYSCONFIG
Hi all
I have one question
How can I change interrupt priority on the am335x board?
I want to change to priority of interrupts 4 (tilcdc,4a100000.ethernet, gp_timer, DM timer 4)
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SYSCONFIG
Hi all
I have one question
How can I change interrupt priority on the am335x board?
I want to change to priority of interrupts 4 (tilcdc,4a100000.ethernet, gp_timer, DM timer 4)
thank you
HI Yordan
I have one question.
I don't find INTC_ILR_X register setting function in the _init omap_init_irq()
=======================================================
static void __init omap_init_irq(u32 base, int nr_irqs,
struct device_node *node)
{
void __iomem *omap_irq_base;
unsigned long nr_of_irqs = 0;
unsigned int nr_banks = 0;
int i, j, irq_base;
omap_irq_base = ioremap(base, SZ_4K);
if (WARN_ON(!omap_irq_base))
return;
irq_base = irq_alloc_descs(-1, 0, nr_irqs, 0);
if (irq_base < 0) {
pr_warn("Couldn't allocate IRQ numbers\n");
irq_base = 0;
}
domain = irq_domain_add_legacy(node, nr_irqs, irq_base, 0,
&irq_domain_simple_ops, NULL);
for (i = 0; i < ARRAY_SIZE(irq_banks); i++) {
struct omap_irq_bank *bank = irq_banks + i;
bank->nr_irqs = nr_irqs;
/* Static mapping, never released */
bank->base_reg = ioremap(base, SZ_4K);
if (!bank->base_reg) {
pr_err("Could not ioremap irq bank%i\n", i);
continue;
}
omap_irq_bank_init_one(bank);
for (j = 0; j < bank->nr_irqs; j += 32)
omap_alloc_gc(bank->base_reg + j, j + irq_base, 32);
nr_of_irqs += bank->nr_irqs;
nr_banks++;
}
pr_info("Total of %ld interrupts on %d active controller%s\n",
nr_of_irqs, nr_banks, nr_banks > 1 ? "s" : "");
}
static void __init omap_irq_bank_init_one(struct omap_irq_bank *bank)
{
unsigned long tmp;
tmp = intc_bank_read_reg(bank, INTC_REVISION) & 0xff;
pr_info("IRQ: Found an INTC at 0x%p (revision %ld.%ld) with %d interrupts\n",
bank->base_reg, tmp >> 4, tmp & 0xf, bank->nr_irqs);
tmp = intc_bank_read_reg(bank, INTC_SYSCONFIG);
tmp |= 1 << 1; /* soft reset */
intc_bank_write_reg(tmp, bank, INTC_SYSCONFIG);
while (!(intc_bank_read_reg(bank, INTC_SYSSTATUS) & 0x1))
/* Wait for reset to complete */;
/* Enable autoidle */
intc_bank_write_reg(1 << 0, bank, INTC_SYSCONFIG);
}
===============================================================
there is no INTC_ILR_X register setting function in the __init omap_irq_bank_init_one()
where is the INTC_ILR_X register setting function?
thank you