I have set VDDSHV4 & VDDSHV7 to 1.8V and VDDSHV3 to 3.3V and have them configured that way in the pin mux tool. I first set GPIO1_16 (pin D27) and GPIO1_17 (pin C28) and then GPIO1_22 thru 25 (pins AC8, AD6, AB8, AB5). Then I went to select GPIO1_4 (pin D15) and got a voltage conflict. Looking at the AM572x_SR2.0_DM I do not see why this won't work. GPIO1_16 (pin D27) and GPIO1_17 (pin C28) are on VDDSHV4 and GPIO1_22 thru 25 (pins AC8, AD6, AB8, AB5) are on VDDSHV7 both of which are 1.8V domains, while GPIO1_4 (pin D15) is on the 3.3V domain VDDSHV3 which is what I need them to be. What does this mean and what do I do to resolve it?