This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x RTC stops when VDD_CORE is switched off.

Hi!

I experienced above problem with my first prototype card whose processor was silicon version 1.0. I got my processor upgraded to silicon version 2.1 (AM3352BZCZ). However, same feature seems to be still present. According to errata (http://www.ti.com/lit/er/sprz360g/sprz360g.pdf) this should have been fixed in silicon revisions 2.0 and 2.1.


Vdd_core and vdd_mpu are switched OFF but vdd_rtc is ON. Is there anything more I should do - or have I anyhow got silicon revision 1.0 in spite of the package markings?

Thanks,

Matti