This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x U-boot Ethernet

hi

I have a ethernet program in the uboot in SDK 06_00_00_00 。

we has a starter kit board with one ethernet port, in uboot the ethernet port is ok。

now We made a new board with two ethernet port, but the old ethernet port can't use. if I remove the another ethernet port , the old ethernet port can use again. It is very odd.

and I also checked using uboot in SDK05, in the new board with two ethernet port, the old ethernet port can use ok!!

so did I miss somtehing to use the uboot in sdk 06? how should I check?

thank you very much!