hi
i have "arago-base-tisdk-image-am335x-evm-20160405224338.rootfs" filesystem as UBI image in NAND flash. can i convert it to initramfs image and flash it with kernel in NAND ?
regarding this already i followed this procedure given in "http://processors.wiki.ti.com/index.php/Sitara_Linux_Program_the_eMMC_on_Beaglebone_Black"
and instead of "tiny flasher system" i used "arago-base-tisdk-image-am335x-evm-20160405224338.rootfs" and made symbolic link to "init.sysvinit" in the top most directory so that kernel can start the filesystem. i have also flashed the uboot, MLO and am335x_evm.dtb also in NAND flash in respective regions but when im booting the image the kernel hangs.
kindly tell me where could be the problem and how can i exercise initramfs using "arago-base-tisdk-image-am335x-evm-20160405224338.rootfs" in NAND in am3358evm