Other Parts Discussed in Thread: AM5728
Hi,
We ware using custom board having am5728 processor. After successful booting i am able to see /dev/fb0 and /dev/video10 device node.
#Output of modetest command
trying to open device 'i915'...failed.
trying to open device 'radeon'...failed.
trying to open device 'nouveau'...failed.
trying to open device 'vmwgfx'...failed.
trying to open device 'omapdrm'...success.[ 1550.097155] omapdss error: HDMI I2C Master Error //What is this error, I am using 2 I2c2 Lines but i am using for hdmi_sda and hdmi_scl signal by doing proper pin muxing in uboot for hdmi.
Encoders:
id crtc type possible crtcs possible clones
25 28 TMDS 0x00000001 0x00000000
Connectors:
id encoder status type size (mm) modes encoders
26 25 connected HDMI-A 0x0 5 25
modes:
name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
1024x768 60 1024 1048 1184 1344 768 771 777 806 flags: nhsync, nvsync; type: driver
800x600 60 800 840 968 1056 600 601 605 628 flags: phsync, pvsync; type: driver
800x600 56 800 824 896 1024 600 601 603 625 flags: phsync, pvsync; type: driver
848x480 60 848 864 976 1088 480 486 494 517 flags: phsync, pvsync; type: driver
640x480 60 640 656 752 800 480 489 492 525 flags: nhsync, nvsync; type: driver
props:
1 EDID:
flags: immutable blob
blobs:
value:
2 DPMS:
flags: enum
enums: On=0 Standby=1 Suspend=2 Off=3
value: 3
I am able to see rotating cube on display while i am running "kmscube" application on default display . But If I want to run stored raw or compressed video using gstreamer or using viddec3test kmscube command i am getting following error.
1. Playing raw video using viddec3test and kmscube application
root@am57xx-evm:~# viddec3test 5sec0.yuv --kmscube --connector 26
0x2c070: Opening Display..
[ 848.872016] omapdss error: HDMI I2C Master Error
Chosen Connector ID = 26
failed to load module: /usr/lib/gbm/gbm_dri.so: cannot open shared object file: No such file or directory
failed to load module: /usr/lib/gbm/gbm_gallium_drm.so: cannot open shared object file: No such file or directory
loaded module: gbm_pvr.so
PVR:(Warning): PVRSRVOpenDCDevice: Warning - 138 returned [80, /bridged_pvr_dc_glue.c]
Using display 0x1 with EGL version 1.4
EGL Version "1.4 build 1.9@2253347"
EGL Vendor "Imagination Technologies"
EGL Extensions "EGL_IMG_client_api_ogl EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_gl_texture_2D_image EGL_KHR_gl_texture_cubemap_image EGL_KHR_gl_renderbuffer_image EGL_KHR_vg_parent_image EGL_IMG_cl_image EGL_KHR_fence_sync EGL_IMG_hibernate_process EGL_WL_bind_wayland_display EGL_KHR_surfaceless_gles2 EGL_NV_post_sub_buffer "
GL Extensions "GL_OES_rgb8_rgba8 GL_OES_depth24 GL_OES_vertex_half_float GL_OES_texture_float GL_OES_texture_half_float GL_OES_element_index_uint GL_OES_mapbuffer GL_OES_fragment_precision_high GL_OES_compressed_ETC1_RGB8_texture GL_OES_EGL_image GL_OES_EGL_image_external GL_OES_required_internalformat GL_OES_depth_texture GL_OES_get_program_binary GL_OES_packed_depth_stencil GL_OES_standard_derivatives GL_OES_vertex_array_object GL_OES_egl_sync GL_OES_texture_npot GL_EXT_multi_draw_arrays GL_EXT_texture_format_BGRA8888 GL_EXT_discard_framebuffer GL_EXT_shader_texture_lod GL_IMG_shader_binary GL_IMG_texture_compression_pvrtc GL_IMG_texture_compression_pvrtc2 GL_IMG_texture_npot GL_IMG_texture_format_BGRA8888 GL_IMG_read_format GL_IMG_program_binary GL_IMG_uniform_buffer_object GL_IMG_multisampled_render_to_texture GL_TI_image_external_raw_video "
Display initialized, Render thread created
0x2c070: Opening Demuxer..
[IMGUTILS @ 0xbec02734] Picture size 0x0 is invalid
[IMGUTILS @ 0xbec0267c] Picture size 0x0 is invalid
[rawvideo @ 0x2d660] Could not find codec parameters (Video: rawvideo, yuv420p)
[rawvideo @ 0x2d660] Estimating duration from bitrate, this may be inaccurate
ERROR:open_file:54: 5sec0.yuv: lavf error -1
2. Playing .mp4 file with viddec3test application
root@am57xx-evm:~# viddec3test test.mp4 --kmscube --connector 26
0x2c070: Opening Display..
[ 1066.839758] omapdss error: HDMI I2C Master Error
Chosen Connector ID = 26
failed to load module: /usr/lib/gbm/gbm_dri.so: cannot open shared object file: No such file or directory //These shared object file sis not available in my file system
failed to load module: /usr/lib/gbm/gbm_gallium_drm.so: cannot open shared object file: No such file or directory//These shared object file sis not available in my file system
loaded module: gbm_pvr.so
PVR:(Warning): PVRSRVOpenDCDevice: Warning - 138 returned [80, /bridged_pvr_dc_glue.c]
Using display 0x1 with EGL version 1.4
EGL Version "1.4 build 1.9@2253347"
EGL Vendor "Imagination Technologies"
EGL Extensions "EGL_IMG_client_api_ogl EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_gl_texture_2D_image EGL_KHR_gl_texture_cubemap_image EGL_KHR_gl_renderbuffer_image EGL_KHR_vg_parent_image EGL_IMG_cl_image EGL_KHR_fence_sync EGL_IMG_hibernate_process EGL_WL_bind_wayland_display EGL_KHR_surfaceless_gles2 EGL_NV_post_sub_buffer "
GL Extensions "GL_OES_rgb8_rgba8 GL_OES_depth24 GL_OES_vertex_half_float GL_OES_texture_float GL_OES_texture_half_float GL_OES_element_index_uint GL_OES_mapbuffer GL_OES_fragment_precision_high GL_OES_compressed_ETC1_RGB8_texture GL_OES_EGL_image GL_OES_EGL_image_external GL_OES_required_internalformat GL_OES_depth_texture GL_OES_get_program_binary GL_OES_packed_depth_stencil GL_OES_standard_derivatives GL_OES_vertex_array_object GL_OES_egl_sync GL_OES_texture_npot GL_EXT_multi_draw_arrays GL_EXT_texture_format_BGRA8888 GL_EXT_discard_framebuffer GL_EXT_shader_texture_lod GL_IMG_shader_binary GL_IMG_texture_compression_pvrtc GL_IMG_texture_compression_pvrtc2 GL_IMG_texture_npot GL_IMG_texture_format_BGRA8888 GL_IMG_read_format GL_IMG_program_binary GL_IMG_uniform_buffer_object GL_IMG_multisampled_render_to_texture GL_TI_image_external_raw_video "
Display initialized, Render thread created
0x2c070: Opening Demuxer..
[aac @ 0x31a20] channel element 2.0 is not allocated
Input #0, mov,mp4,m4a,3gp,3g2,mj2, from 'test.mp4':
Metadata:
major_brand : mp42
minor_version : 0
compatible_brands: mp42mp41isomiso2
creation_time : 2016-06-18 13:08:37
Duration: 00:04:29.12, start: 0.000000, bitrate: 5952 kb/s
Stream #0.0(eng): Video: h264 (Baseline), yuv420p, 1920x1200, 5817 kb/s, 29.97 fps, 3k tbn
Metadata:
creation_time : 2016-06-18 13:08:37
Stream #0.1(eng): Audio: aac, 44100 Hz, stereo, fltp, 128 kb/s
Metadata:
creation_time : 2016-06-18 13:08:37
initializing bitstream filter
0x2c070: infile=test.mp4, width=1920, height=1200
0x2c070: padded_width=2048, padded_height=1296, num_buffers=6
get_buffers not supported!
0x2c070: uv_offset=2654208
0x2c070: Opening Engine..
MmRpc_create: Error: open failed, name=/dev/rpmsg-dce //What is this error, This node is not in my filesystem
ERROR:decoder_open:207: 0x2c070: could not open engine
/home/gtbldadm/processor-sdk-linux-fido-build/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-linux-gnueabi/libdce/3.00.08.02-r0/git/libdce.c:198: dce_ipc_init Error: ERROR: Failed eError == DCE_EOK error val -4/home/gtbldadm/processor-sdk-linux-fido-build/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-linux-gnueabi/libdce/3.00.08.02-r0/git/libdce.c:276: Engine_open Error: ERROR: Failed dce_ipc_init(coreIdx) == DCE_ Failedopen Error: ERROR: Failed
3. Playing raw yuv file using gstreamer
evm:~# gst-launch-1.0 filesrc location=5sec0.yuv ! v4l2sink device=/dev/video10
Setting pipeline to PAUSED ...
ERROR: Pipeline doesn't want to pause.src location=5sec0.yuv ! v4l2sink device=/
ERROR: from element /GstPipeline:pipeline0/GstV4l2Sink:v4l2sink0: Device '/dev/video10' is not a output device.//why its giving not a aoutput device error
Additional debug info:
/home/gtbldadm/processor-sdk-linux-fido-build/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-linux-gnueabi/gstreamer1.0-plugins-good/1.2.3-r0-arago1/gst-plugins-good-1.2.3/sys/v4l2/v4l2_calls.c(594): gst_v4l2_open (): /GstPipeline:pipeline0/GstV4l2Sink:v4l2sink0:
Capabilities: 0x84204000
Setting pipeline to NULL ...
Freeing pipeline ...
Thanks & Regards
Abhishek