Hello, my customer asked me the following, and I quote:
I'm trying to do on Ubuntu 14.04 LTS operating system as follows:
Download sdk:
software-dl.ti.com/.../index_FDS.html
Declared support for the ICE in this release:
processors.wiki.ti.com/.../Processor_SDK_Linux_Release_Notes
I create the SD card via the create-sdcard script compiled binaries (prebuilt images):
processors.wiki.ti.com/.../Processor_SDK_Linux_create_SD_card_script
As a result, in the boot SD card are copied MLO files and u-boot.img.
I insert an SD card into the card (jumpers are set to boot from the SD card) and reloads fee.
As a result, the terminal (connected via minicom utility) displays a message stating that the application has been found and downloaded the demo application from the SPI flash.
Next, I rename MLO in the APP, to StarterWare downloaded it, and then the boot process hangs:
"Image copy Successful, Executing Application ..."