This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: 8-bit data access to PCIe mapped domain

Part Number: AM5728


Hi,

Does the 8bit read access of memory mapped in PCIe of AM5728 support it?
Environment
AM5728 :RC
External device: EP
It has been mapped with DDR3 memory region.

① 0x0102_0304_0506_0708_090A
When it is read the data written in the memory mentioned above by 8bit read access,  it is read as follows.
② 0x0100_0000_0500_0000_0900

When I read by 32bit read access, normal data ① is readable.

Best Regards,
Shigehiro Tsuda