This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXIDK5728: SD card boot fails



We have purchased one TI TMDXIDK5728 board, it can’t boot up with the incoming SD card. The SD card can boot up other same board.

 

Stop at here, is this a hardware problem? Hope can get some help from you. Thanks in advance.

 

U-Boot SPL 2016.05-00039-gb43cf45 (Nov 09 2016 - 16:07:40)
DRA752-GP ES2.0
Trying to boot from MMC1
i2c_write: error waiting for data ACK (status=0x116)
tps65903x: could not set LDO1 voltage.
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
reading u-boot.img
No matching DT out of these options:
   am57xx-beagle-x15
   am572x-idk
   am571x-idk
Failed to mount ext2 filesystem...
spl_load_image_ext_os: ext4fs mount err - 0
Failed to mount ext2 filesystem...
spl_load_image_ext: ext4fs mount err - 0