Hi,
We're using the Cloud version (version 4 I think) of the TI pin mux tool for the AM5728 (AM5728_SR2.0). When I add HDMI, I get voltage conflict warnings. I need to know if this is a real issue with our design or just a tool artifact.
Here's a screenshot of the pin mux tool showing the warnings.
The HDMI pins supplied by vdda_hdmi are all fixed at 1.8V by spec so in the Preferred Voltage setting in the pin mux tool, I set it to 1.8V, otherwise I get voltage conflict warnings about the HDMI pins supplied by vdda_hdmi being at 3.3V. However, by setting Preferred Voltage to 1.8V, I now get voltage conflict warnings regarding the other HDMI pins that are powered by vddshv3 which is set to 3.3V. I can't change vddshv3 to 1.V because it has so may other pins on that power group that need to be 3.3V.
It seems to me, even though the HDMI pins that are powered by vdda_hdmi are at 1.8V, that I should still be able to power the other HDMI pins powered by vddshv3 at 3.3V. The tools indicates this is a conflict.
What I need is to know if this is a real voltage conflict in our design or just a tool nuance.
Thanks