This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Configuring 4GB DDR3L

Part Number: AM5728


We just received our custom board, and we have 4 GB of DDR3L with part number MT41K512M16HA, so there are 4 ICs total. Our problem is that Uboot/Linux only show that we have 2 GB of RAM.

Uboot works, booting into Linux works, display, ethernet, etc all work, but our memory access is limited to 2 GB.

What we're interested in doing is having Q2 access 2 GB of memory through its 1 GB window and having Q3 2 GB of memory through its 1 GB window. We want to have EMIF 1 and 2 to be interleaved on both Q2 and Q3. Do we need to set up all 4 LISA registers, or just 2 LISA registers, as seen in most examples? Does it matter which registers we use? Is this even the right way to think about this?

Is there a working example of interleaving both EMIF 1 and 2 to enable access to 4 GB of RAM?

We've looked at the DRA74x EVM uboot settings, but the register settings don't make much sense, and the settings didn't work for us. We could use some support on this.

  • The software team have been notified. They will respond here.
  • Hi,

    Apologies for the delayed response.
    See the following thread:
    e2e.ti.com/.../552861

    Best Regards,
    Yordan
  • Hi Yordan,


    We have tried everything suggested in that and other threads. We checked that the kernel enables LPAE, verified that the higher memory interleaving was enabled in MA_PRIORITY, and we set the LISA map to enable interleaving on the lower 2 GB. I also used devmem2 to read the MA_PRIORITY register and the LISA map registers to verify they are set. The LISA map registers are set to:

        .dmm_lisa_map_0 = 0x0,
        .dmm_lisa_map_1 = 0x0,
        .dmm_lisa_map_2 = 0x80740300,
        .dmm_lisa_map_3 = 0xFF020100,
        .is_ma_present = 0x1

    Is there something we need to do in the MMU to let it know it can access a higher memory space? Or anything else we might be missing?

  • Hi,

    Ok, can you download the latest automotive processor SDK, which supports www.ti.com/.../j6evm5777. The DRA75x EVM uses 4GB RAM, 2GB on each EMIF. And the architecture of the automotive DRA75x & AM57x is quite the same, so look at the lisa map configurations there. The SDK is located here:
    processors.wiki.ti.com/.../Category:Processor_SDK_Linux_Automotive

    Best Regards,
    Yordan
  • We've already looked at that SDK, and we have verified that our LISA map is the same. The LISA map is only for the lower 2 GB of memory, right? So that still doesn't help us enable the upper 2 GB. Or maybe the upper 2 GB is enabled, but U-Boot and Linux aren't aware of it because only the MPU can access it? Is there any way to determine if the MPU is able to use the upper 2 GB of RAM?

  • We found what we were missing! We went back and looked at the board file for the DRA75x EVM, and we noticed that it had a different dram_init_banksize function, which tells uboot about the second area of memory starting at 0x200000000.Here is the function in case anyone else comes looking:

    void dram_init_banksize(void)
    {
        u64 ram_size;

        ram_size = board_ti_get_emif_size();

        gd->bd->bi_dram[0].start = CONFIG_SYS_SDRAM_BASE;
        gd->bd->bi_dram[0].size = get_effective_memsize();
        if (ram_size > CONFIG_MAX_MEM_MAPPED) {
            gd->bd->bi_dram[1].start = 0x200000000;
            gd->bd->bi_dram[1].size = ram_size - CONFIG_MAX_MEM_MAPPED;
        }
    }

    We cheated and just set ram_size to equal 0x100000000 and changed the types of bi_dram.start/stop to u64, but maybe the more correct way would be to configure the system as a 64 bit system?

  • Another thing for a successful 4GB DDR3 configuration is to NOT enable CONFIG_ARMV7_LPAE in u-boot.  Enabling CONFIG_ARMV7_LPAE in u-boot with the dram_init_banksize update above would cause the system to "hang".  In our case, dram_init_banksize executes the following:

                gd->bd->bi_dram[0].start = CONFIG_SYS_SDRAM_BASE;
                gd->bd->bi_dram[0].size = get_effective_memsize();
                gd->bd->bi_dram[1].start = 0x200000000;
                gd->bd->bi_dram[1].size = CONFIG_MAX_MEM_MAPPED;   /* we defined CONFIG_MAX_MEM_MAPPED as 0x80000000 */

    Also remember to update include\asm-generic\u-boot.h to change the types of start and size to u64:

    struct {   /* RAM configuration */
      u64 start;
      u64 size;
     } bi_dram[CONFIG_NR_DRAM_BANKS];   /* we defined CONFIG_NR_DRAM_BANKS as 2 */


    The kernel DOES need CONFIG_ARM_LPAE=y for the 4GB to be recognized.

  • We do have LPAE enabled in u-boot, and it hasn't caused us problems. We did also change the types of start and size in the bi_dram struct, so maybe doing that removes the problems caused by enabling LPAE?