Part Number: AM3352
Tool/software: Linux
Hi.
I use board with custom hardware, that connect WiFi over USB to am3352. I use mainline Linux 4.8.17.
In my board schematics only USB signal lines (USB1_DM and USB1_DP) connected from CPU to WiFI (but not USB Power line, USB +5V connected from other power supply, and not connected with am3352).
In result I see USB error in dmesg:
[ 734.531123] musb-hdrc musb-hdrc.0.auto: VBUS_ERROR in a_wait_vrise (81, <SessEnd), retry #1, port1 0008050c
[ 734.683550] musb-hdrc musb-hdrc.0.auto: VBUS_ERROR in a_wait_vrise (81, <SessEnd), retry #2, port1 0008050c
[ 734.835977] musb-hdrc musb-hdrc.0.auto: VBUS_ERROR in a_wait_vrise (81, <SessEnd), retry #3, port1 0008050c
[ 734.988398] musb-hdrc musb-hdrc.0.auto: VBUS_ERROR in a_wait_vrise (80, <SessEnd), retry #3, port1 0008050c
And USB does not work.
lsusb just show internal hub:
# lsusb
Bus 001 Device 001: ID 1d6b:0002
My device tree (USB part):
How I can fix USB?