Part Number: AM5726
Tool/software: Linux
Hello,
I need to do power consumption at u-boot level as well as at kernel level.
How can I do the lowest OPP in u-boot?
At kernel level, I changed the governor in powersave mode.
Here powersave mode is running at 1GHz and maximum is 1.5GHz.
If I want to add lower than 1 GHz support in powersave mode how can I do?
I need to compromise boot time while OPP is low, but when the board will boot up, I will change the governor from powersave mode to ondemand mode.
Please do the needful.
Regards,
-- Ronak