Part Number: AM3357
Tool/software: Linux
Hello Sir,
Our custom board based on AM335x evaluation board has OTG on USB0 and RF module on USB1. USB1 is working fine.
we have issue with USB0. we have supplied 5v through power switch.
we followed this schematic
we are able to see 5v at input of the power switch but we are not able to see at the USB0_VBUS.
when i do,
root@am335x-evm:~# lsusb
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation
Bus 002 Device 002: ID 1e2d:0061
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation
root@am335x-evm:/# cat /proc/interrupts
CPU0
16: 19172 INTC 68 Level gp_timer
19: 1 INTC 78 Level wkup_m3_txev
20: 487 INTC 12 Level 49000000.edma_ccint
22: 0 INTC 14 Level 49000000.edma_ccerrint
26: 0 INTC 96 Level 44e07000.gpio
33: 0 44e07000.gpio 6 Edge 48060000.mmc cd
59: 0 INTC 98 Level 4804c000.gpio
92: 0 INTC 32 Level 481ac000.gpio
125: 0 INTC 62 Level 481ae000.gpio
158: 566 INTC 72 Level 44e09000.serial
160: 824 INTC 70 Level 44e0b000.i2c
161: 0 INTC 71 Level 4802a000.i2c
162: 11 INTC 64 Level mmc1
163: 13 INTC 29 Level mmc0
165: 0 INTC 77 Level wkup_m3
171: 0 INTC 75 Level rtc0
172: 0 INTC 76 Level rtc0
174: 0 INTC 41 Level 4a100000.ethernet
175: 0 INTC 42 Level 4a100000.ethernet
177: 0 INTC 4 Level 48080000.elm
179: 0 INTC 16 Level TI-am335x-tsc, TI-am335x-adc
180: 0 INTC 100 Level gpmc
181: 12 INTC 109 Level 53100000.sham
183: 0 INTC 111 Level 48310000.rng
188: 0 INTC 18 Level musb-hdrc.0.auto
189: 125 INTC 19 Level musb-hdrc.1.auto
190: 2 INTC 17 Level 47400000.dma-controller
Err: 0
root@am335x-evm:/# cat /proc/driver/
here i am not getting musb-hdrc.0 and musb-hdrc.1
Sir, please suggest is there anything that i have to do from software or we need to change anything in hardware.
i am using tisdk 03.03.00.04