Part Number: PRU-SWPKG
Hi,
Since the PRUSS 0 does not have an explicit PRU Shared memory available on AM437x I am trying to use PRU DMEM to share variables across the two PRU cores. I have added a pragma directive for DATA_SECTION in both the C files (PRU0 and PRU1 code) and also specified it in the linker file. Both '.map' files show the same address location and space for the variable but I don't see the variable being updated. The way i am checking this is that as soon as the PRU1 updates the variable, PRU0 flashes an led but that doesn't look like it is working.
Here are the relevant sections:
C file declaration in PRU0.c and PRU1.c (identical in both):
#pragma DATA_SECTION(max_count, ".max_count") volatile far uint32_t max_count = 0;
The .map file:
PRU0
.max_count
* 1 00002fe0 00000004 UNINITIALIZED
00002fe0 00000004 PRU0.object (.max_count)
PRU1
.max_count
* 1 00002fe0 00000004 UNINITIALIZED
00002fe0 00000004 PRU_pidSendData.object (.max_count)
And I have also attached the linker file.
/****************************************************************************/
/* AM437x_PRU_SS0.cmd */
/* Copyright (c) 2015 Texas Instruments Incorporated */
/* */
/* Description: This file is a linker command file that can be used for */
/* linking PRU programs built with the C compiler and */
/* the resulting .out file on an AM437x device. */
/****************************************************************************/
-cr /* Link using C conventions */
/* Specify the System Memory Map */
MEMORY
{
PAGE 0:
PRU_IMEM : org = 0x00000000 len = 0x00001000 /* 4kB PRU-ICSS0 Instruction RAM */
PAGE 1:
/* RAM */
PRU_DMEM_0_1 : org = 0x00000000 len = 0x00001000 CREGISTER=24 /* 4kB PRU Data RAM 0_1 */
PRU_DMEM_1_0 : org = 0x00002000 len = 0x00000fe0 CREGISTER=25 /* 4kB PRU Data RAM 1_0 */
SHAREDMEM : org = 0x00002fe0 len = 0x00000004
DDR : org = 0x80000000 len = 0x00000100 CREGISTER=31
L3OCMC : org = 0x40000000 len = 0x00010000 CREGISTER=30
PAGE 2:
/* Peripherals */
PRU_CFG : org = 0x00026000 len = 0x00000120 CREGISTER=4
PRU_ECAP : org = 0x00030000 len = 0x00000060 CREGISTER=3
PRU_IEP : org = 0x0002E000 len = 0x0000031C CREGISTER=26
PRU_INTC : org = 0x00020000 len = 0x00001504 CREGISTER=0
PRU_UART : org = 0x00028000 len = 0x00000038 CREGISTER=7
DCAN0 : org = 0x481CC000 len = 0x000001E8 CREGISTER=14
DCAN1 : org = 0x481D0000 len = 0x000001E8 CREGISTER=15
DMTIMER2 : org = 0x48040000 len = 0x0000005C CREGISTER=1
PWMSS0 : org = 0x48300000 len = 0x000002C4 CREGISTER=18
PWMSS1 : org = 0x48302000 len = 0x000002C4 CREGISTER=19
PWMSS2 : org = 0x48304000 len = 0x000002C4 CREGISTER=20
GEMAC : org = 0x4A100000 len = 0x0000128C CREGISTER=9
I2C1 : org = 0x4802A000 len = 0x000000D8 CREGISTER=2
I2C2 : org = 0x4819C000 len = 0x000000D8 CREGISTER=17
MBX0 : org = 0x480C8000 len = 0x00000140 CREGISTER=22
MCASP0_DMA : org = 0x46000000 len = 0x00000100 CREGISTER=8
MCSPI0 : org = 0x48030000 len = 0x000001A4 CREGISTER=6
MCSPI1 : org = 0x481A0000 len = 0x000001A4 CREGISTER=16
MMCSD0 : org = 0x48060000 len = 0x00000300 CREGISTER=5
SPINLOCK : org = 0x480CA000 len = 0x00000880 CREGISTER=23
TPCC : org = 0x49000000 len = 0x00001098 CREGISTER=29
UART1 : org = 0x48022000 len = 0x00000088 CREGISTER=11
UART2 : org = 0x48024000 len = 0x00000088 CREGISTER=12
RSVD10 : org = 0x48318000 len = 0x00000100 CREGISTER=10
RSVD13 : org = 0x48310000 len = 0x00000100 CREGISTER=13
RSVD21 : org = 0x00032400 len = 0x00000100 CREGISTER=21
RSVD27 : org = 0x00032000 len = 0x00000100 CREGISTER=27
}
/* Specify the sections allocation into memory */
SECTIONS {
/* Forces _c_int00 to the start of PRU IRAM. Not necessary when loading
an ELF file, but useful when loading a binary */
.text:_c_int00* > 0x0, PAGE 0
.text > PRU_IMEM, PAGE 0
.stack > PRU_DMEM_0_1, PAGE 1
.bss > PRU_DMEM_0_1, PAGE 1
.cio > PRU_DMEM_0_1, PAGE 1
.data > PRU_DMEM_0_1, PAGE 1
.switch > PRU_DMEM_0_1, PAGE 1
.sysmem > PRU_DMEM_0_1, PAGE 1
.cinit > PRU_DMEM_0_1, PAGE 1
.rodata > PRU_DMEM_0_1, PAGE 1
.rofardata > PRU_DMEM_0_1, PAGE 1
.farbss > PRU_DMEM_0_1, PAGE 1
.fardata > PRU_DMEM_0_1, PAGE 1
.resource_table > PRU_DMEM_0_1, PAGE 1
.max_count > SHAREDMEM, PAGE 1
}
Is there something else that needs to be declared?