Part Number: AM3352
Tool/software: Linux
Hello everyone,
I have a custom board using AM3352 processor and I´m facing a problem while trying to use GPIO0_2, GPIO0_3, GPIO0_4 and GPIO0_5 as regular GPIO pins. GPI0_6 and GPIO0_7 from GPIO0 bank are perfectly working!
Previously I´ve used these and other pins as SPI port to connect my board to a SPI TFT Display. So, my "hardware connection" is tested (at least I believe so).
I´m using TI SDK 03.03.00.04, with Linux 4.4.31. My device tree is based on am335x-evm.dts (with a few modifications). I´ve already tried to disable SPI on Kernel and Device Tree (thinking that these ports are allocated to SPI), with no success. I can´t change pin state from GPIO-3 and GPIO-5 (programmed as output) or read something different from ZERO on GPIO-2 and GPIO-4. I still believe that these ports are being used by Linux to other pourpose, but I don´t how to check or change it.
Here a few debug information:
~ # cat /sys/kernel/debug/gpio GPIOs 0-31, platform/44e07000.gpio, gpio: gpio-2 ( |sysfs ) in lo gpio-3 ( |sysfs ) out lo gpio-4 ( |sysfs ) in lo gpio-5 ( |sysfs ) out lo gpio-6 ( |sysfs ) out hi gpio-7 ( |sysfs ) out lo
~ # cat /lib/modules/$(uname -r)/modules.builtin | grep spi ~ #
*****************************************************************************************************************************
Some information from my DEVICE TREE:
gpio_0_pins: gpio_0_pins {
pinctrl-single,pins = <
0x150 ( PIN_INPUT | MUX_MODE7 ) /* (A17) spi0_sclk.gpio0[2] */
0x154 ( PIN_OUTPUT | MUX_MODE7 ) /* (B17) spi0_d0.gpio0[3] */
0x158 ( PIN_INPUT | MUX_MODE7 ) /* (B16) spi0_d1.gpio0[4] */
0x15c ( PIN_OUTPUT | MUX_MODE7 ) /* (A16) spi0_cs0.gpio0[5] */
0x160 ( PIN_INPUT | MUX_MODE7 ) /* (C15) spi0_cs1.gpio0[6] */
0x164 ( PIN_INPUT | MUX_MODE7 ) /* (C18) eCAP0_in_PWM0_out.gpio0[7] */
/*0x1b0 ( PIN_INPUT | MUX_MODE7 )*/ /* (A15) xdma_event_intr0.gpio0[19] */
/*0x1b4 ( PIN_INPUT | MUX_MODE7 )*/ /* (D14) xdma_event_intr1.gpio0[20] */
>;
};
&spi0 {
status = "disabled";
};
Does anyone have any ideia? I´m stucked on this issue over a week...
Thanks!
Fernando Pina